PLCamera.TimerSequenceEntrySelectorEnum Class#
Visibility: Guru
Selecting Parameters: TimerSequenceTimerSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TimerSequenceEntrySelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.TimerSequenceEntrySelectorEnum | Initializes a new instance of the PLCamera.TimerSequenceEntrySelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Entry1 | ||
Entry10 | ||
Entry11 | ||
Entry12 | ||
Entry13 | ||
Entry14 | ||
Entry15 | ||
Entry16 | ||
Entry2 | ||
Entry3 | ||
Entry4 | ||
Entry5 | ||
Entry6 | ||
Entry7 | ||
Entry8 | ||
Entry9 | ||
名前 | The full name of TimerSequenceEntrySelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TimerSequenceEntrySelector (Overrides Object.ToString()()()().) |
PLCamera.TimerSequenceEntrySelectorEnum.ToString Method#
The full name of TimerSequenceEntrySelector
Return Value#
Type: String
Returns the full name of TimerSequenceEntrySelector
PLCamera.TimerSequenceEntrySelectorEnum Constructor#
Initializes a new instance of the PLCamera.TimerSequenceEntrySelectorEnum class
PLCamera.TimerSequenceEntrySelectorEnum.Entry1 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry10 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry11 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry12 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry13 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry14 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry15 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry16 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry2 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry3 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry4 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry5 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry6 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry7 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry8 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry9 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Name Property#
The full name of TimerSequenceEntrySelector