PLCamera.BslSerialParityEnum Class#
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslSerialParityEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslSerialParityEnum | Initializes a new instance of the PLCamera.BslSerialParityEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Even | An even parity check is performed. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
名前 | The full name of BslSerialParity (Overrides ParameterListEnum.Name.) | |
None | No parity check is performed. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Odd | An odd parity check is performed. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslSerialParity (Overrides Object.ToString()()()().) |
PLCamera.BslSerialParityEnum.ToString Method#
The full name of BslSerialParity
Return Value#
Type: String
Returns the full name of BslSerialParity
PLCamera.BslSerialParityEnum Constructor#
Initializes a new instance of the PLCamera.BslSerialParityEnum class
PLCamera.BslSerialParityEnum.Even Property#
An even parity check is performed.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialParityEnum.Name Property#
The full name of BslSerialParity
PLCamera.BslSerialParityEnum.None Property#
No parity check is performed.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialParityEnum.Odd Property#
An odd parity check is performed.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress