PLCamera.SequenceAddressBitSourceEnum Class#
Applies to: CameraLink and GigE
Visibility: Guru
Selected by: SequenceAddressBitSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.SequenceAddressBitSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.SequenceAddressBitSourceEnum | Initializes a new instance of the PLCamera.SequenceAddressBitSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
CC1 | The selected bit of the sequence set address can be set using the CC1 signal. Applies to: CameraLink and GigE | |
CC2 | The selected bit of the sequence set address can be set using the CC2 signal. Applies to: CameraLink and GigE | |
CC3 | The selected bit of the sequence set address can be set using the CC3 signal. Applies to: CameraLink and GigE | |
CC4 | The selected bit of the sequence set address can be set using the CC4 signal. Applies to: CameraLink and GigE | |
Line1 | The selected bit of the sequence set address can be set using Line 1. Applies to: CameraLink and GigE | |
Line2 | The selected bit of the sequence set address can be set using Line 2. Applies to: CameraLink and GigE | |
Line3 | The selected bit of the sequence set address can be set using Line 3. Applies to: CameraLink and GigE | |
Line4 | The selected bit of the sequence set address can be set using Line 4. Applies to: CameraLink and GigE | |
Line5 | The selected bit of the sequence set address can be set using Line 5. Applies to: CameraLink and GigE | |
Line6 | The selected bit of the sequence set address can be set using Line 6. Applies to: CameraLink and GigE | |
Line7 | The selected bit of the sequence set address can be set using Line 7. Applies to: CameraLink and GigE | |
Line8 | The selected bit of the sequence set address can be set using Line 8. Applies to: CameraLink and GigE | |
名前 | The full name of SequenceAddressBitSource (Overrides ParameterListEnum.Name.) | |
VInput1 | Selects Virtual Input 1 as the source for the selected bit of the sequence set address. Applies to: CameraLink and GigE | |
VInput2 | Selects Virtual Input 2 as the source for the selected bit of the sequence set address. Applies to: CameraLink and GigE | |
VInput3 | Selects Virtual Input 3 as the source for the selected bit of the sequence set address. Applies to: CameraLink and GigE | |
VInput4 | Selects Virtual Input 4 as the source for the selected bit of the sequence set address. Applies to: CameraLink and GigE | |
VInputDecActive | Selects Virtual Input Decoder Active as the source for the selected bit of the sequence set address. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of SequenceAddressBitSource (Overrides Object.ToString()()()().) |
PLCamera.SequenceAddressBitSourceEnum.ToString Method#
The full name of SequenceAddressBitSource
Return Value#
Type: String
Returns the full name of SequenceAddressBitSource
PLCamera.SequenceAddressBitSourceEnum Constructor#
Initializes a new instance of the PLCamera.SequenceAddressBitSourceEnum class
PLCamera.SequenceAddressBitSourceEnum.CC1 Property#
The selected bit of the sequence set address can be set using the CC1 signal.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.CC2 Property#
The selected bit of the sequence set address can be set using the CC2 signal.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.CC3 Property#
The selected bit of the sequence set address can be set using the CC3 signal.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.CC4 Property#
The selected bit of the sequence set address can be set using the CC4 signal.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line1 Property#
The selected bit of the sequence set address can be set using Line 1.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line2 Property#
The selected bit of the sequence set address can be set using Line 2.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line3 Property#
The selected bit of the sequence set address can be set using Line 3.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line4 Property#
The selected bit of the sequence set address can be set using Line 4.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line5 Property#
The selected bit of the sequence set address can be set using Line 5.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line6 Property#
The selected bit of the sequence set address can be set using Line 6.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line7 Property#
The selected bit of the sequence set address can be set using Line 7.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Line8 Property#
The selected bit of the sequence set address can be set using Line 8.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.Name Property#
The full name of SequenceAddressBitSource
PLCamera.SequenceAddressBitSourceEnum.VInput1 Property#
Selects Virtual Input 1 as the source for the selected bit of the sequence set address.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.VInput2 Property#
Selects Virtual Input 2 as the source for the selected bit of the sequence set address.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.VInput3 Property#
Selects Virtual Input 3 as the source for the selected bit of the sequence set address.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.VInput4 Property#
Selects Virtual Input 4 as the source for the selected bit of the sequence set address.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSourceEnum.VInputDecActive Property#
Selects Virtual Input Decoder Active as the source for the selected bit of the sequence set address.
Applies to: CameraLink and GigE