PLCamera.GevGVSPExtendedIDModeEnum Class#
Applies to: GigE and ace 2 GigE
Visibility: Expert
Selected by: GevStreamChannelSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.GevGVSPExtendedIDModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.GevGVSPExtendedIDModeEnum | Initializes a new instance of the PLCamera.GevGVSPExtendedIDModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of GevGVSPExtendedIDMode (Overrides ParameterListEnum.Name.) | |
Off | The Extended ID mode is switched off. Applies to: GigE and ace 2 GigE | |
その | The Extended ID mode is switched on. Applies to: GigE and ace 2 GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of GevGVSPExtendedIDMode (Overrides Object.ToString()()()().) |
PLCamera.GevGVSPExtendedIDModeEnum.ToString Method#
The full name of GevGVSPExtendedIDMode
Return Value#
Type: String
Returns the full name of GevGVSPExtendedIDMode
PLCamera.GevGVSPExtendedIDModeEnum Constructor#
Initializes a new instance of the PLCamera.GevGVSPExtendedIDModeEnum class
PLCamera.GevGVSPExtendedIDModeEnum.Name Property#
The full name of GevGVSPExtendedIDMode
PLCamera.GevGVSPExtendedIDModeEnum.Off Property#
The Extended ID mode is switched off.
Applies to: GigE and ace 2 GigE
PLCamera.GevGVSPExtendedIDModeEnum.On Property#
The Extended ID mode is switched on.
Applies to: GigE and ace 2 GigE