PLCamera.TriggerSourceEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
Selected by: TriggerSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TriggerSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.TriggerSourceEnum | Initializes a new instance of the PLCamera.TriggerSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Action1 | The source signal for the selected trigger is set to action command signal 1. Applies to: CamEmu, CameraLink, GigE and ace 2 GigE | |
Action2 | The source signal for the selected trigger is set to action command signal 2. Applies to: CameraLink, GigE and ace 2 GigE | |
Action3 | The source signal for the selected trigger is set to action command signal 3. Applies to: CameraLink and GigE | |
Action4 | The source signal for the selected trigger is set to action command signal 4. Applies to: CameraLink and GigE | |
CC1 | The source signal for the selected trigger is set to CC1. Applies to: CameraLink and GigE | |
CC2 | The source signal for the selected trigger is set to CC2. Applies to: CameraLink and GigE | |
CC3 | The source signal for the selected trigger is set to CC3. Applies to: CameraLink and GigE | |
CC4 | The source signal for the selected trigger is set to CC4. Applies to: CameraLink and GigE | |
Counter1Active | The Counter 1 Active trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter1End | The Counter 1 End trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter1Start | The Counter 1 Start trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter2Active | The Counter 2 Active trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter2End | The Counter 2 End trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter2Start | The Counter 2 Start trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
CxpTrigger0 | The CXP Trigger 0 trigger can be configured. Applies to: boost CoaXPress | |
CXPTrigger0 | The CXP Trigger 0 trigger can be configured. Applies to: boost_V_CoaXPress | |
CxpTrigger1 | The CXP Trigger 1 trigger can be configured. Applies to: boost CoaXPress | |
FrequencyConverter | The source signal for the selected trigger is set to the frequency converter module. Applies to: CameraLink and GigE | |
Line1 | The source signal for the selected trigger is set to Line 1. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
Line2 | The source signal for the selected trigger is set to Line 2. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
Line3 | The source signal for the selected trigger is set to Line 3. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Line4 | The source signal for the selected trigger is set to Line 4. Applies to: CameraLink, GigE, ace USB and dart 2 USB | |
Line5 | The source signal for the selected trigger is set to Line 5. Applies to: CameraLink and GigE | |
Line6 | The source signal for the selected trigger is set to Line 6. Applies to: CameraLink and GigE | |
Line7 | The source signal for the selected trigger is set to Line 7. Applies to: CameraLink and GigE | |
Line8 | The source signal for the selected trigger is set to Line 8. Applies to: CameraLink and GigE | |
名前 | The full name of TriggerSource (Overrides ParameterListEnum.Name.) | |
PeriodicSignal1 | The source signal for the selected trigger is set to Periodic Signal 1. Applies to: CamEmu and ace 2 GigE | |
ShaftEncoderModuleOut | The source signal for the selected trigger is set to the shaft encoder module. Applies to: CameraLink and GigE | |
ソフトウェア | The source signal for the selected trigger is set to software triggering. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
SoftwareSignal1 | The source signal for the selected trigger is set to software signal 1. Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
SoftwareSignal2 | The source signal for the selected trigger is set to software signal 2. Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
SoftwareSignal3 | The source signal for the selected trigger is set to software signal 3. Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Timer1Active | The Timer 1 Active trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer1End | The Timer 1 End trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer1Start | This enumeration value sets the signal source for the selected trigger to timer 1 start. Applies to: CameraLink and GigE | |
Timer2Active | The Timer 2 Active trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer2End | The Timer 2 End trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
UserOutput1 | This enumeration value sets the signal source for the selected trigger to user output 1. Applies to: CameraLink and GigE | |
UserOutput2 | This enumeration value sets the signal source for the selected trigger to user output 2. Applies to: CameraLink and GigE | |
VInput1 | Sets the signal source for the selected trigger to Virtual Input 1. Applies to: CameraLink and GigE | |
VInput2 | Sets the signal source for the selected trigger to Virtual Input 2. Applies to: CameraLink and GigE | |
VInput3 | Sets the signal source for the selected trigger to Virtual Input 3. Applies to: CameraLink and GigE | |
VInput4 | Sets the signal source for the selected trigger to Virtual Input 4. Applies to: CameraLink and GigE | |
VInputDecActive | Sets the signal source for the selected trigger to Virtual Input Decoder Active. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerSource (Overrides Object.ToString()()()().) |
PLCamera.TriggerSourceEnum.ToString Method#
The full name of TriggerSource
Return Value#
Type: String
Returns the full name of TriggerSource
PLCamera.TriggerSourceEnum Constructor#
Initializes a new instance of the PLCamera.TriggerSourceEnum class
PLCamera.TriggerSourceEnum.Action1 Property#
The source signal for the selected trigger is set to action command signal 1.
Applies to: CamEmu, CameraLink, GigE and ace 2 GigE
PLCamera.TriggerSourceEnum.Action2 Property#
The source signal for the selected trigger is set to action command signal 2.
Applies to: CameraLink, GigE and ace 2 GigE
PLCamera.TriggerSourceEnum.Action3 Property#
The source signal for the selected trigger is set to action command signal 3.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Action4 Property#
The source signal for the selected trigger is set to action command signal 4.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.CC1 Property#
The source signal for the selected trigger is set to CC1.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.CC2 Property#
The source signal for the selected trigger is set to CC2.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.CC3 Property#
The source signal for the selected trigger is set to CC3.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.CC4 Property#
The source signal for the selected trigger is set to CC4.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Counter1Active Property#
The Counter 1 Active trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Counter1End Property#
The Counter 1 End trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Counter1Start Property#
The Counter 1 Start trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Counter2Active Property#
The Counter 2 Active trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Counter2End Property#
The Counter 2 End trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Counter2Start Property#
The Counter 2 Start trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.CXPTrigger0 Property#
The CXP Trigger 0 trigger can be configured.
Applies to: boost_V_CoaXPress
PLCamera.TriggerSourceEnum.CxpTrigger1 Property#
The CXP Trigger 1 trigger can be configured.
Applies to: boost CoaXPress
PLCamera.TriggerSourceEnum.FrequencyConverter Property#
The source signal for the selected trigger is set to the frequency converter module.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Line1 Property#
The source signal for the selected trigger is set to Line 1.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.TriggerSourceEnum.Line2 Property#
The source signal for the selected trigger is set to Line 2.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.TriggerSourceEnum.Line3 Property#
The source signal for the selected trigger is set to Line 3.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Line4 Property#
The source signal for the selected trigger is set to Line 4.
Applies to: CameraLink, GigE, ace USB and dart 2 USB
PLCamera.TriggerSourceEnum.Line5 Property#
The source signal for the selected trigger is set to Line 5.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Line6 Property#
The source signal for the selected trigger is set to Line 6.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Line7 Property#
The source signal for the selected trigger is set to Line 7.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Line8 Property#
The source signal for the selected trigger is set to Line 8.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Name Property#
The full name of TriggerSource
PLCamera.TriggerSourceEnum.PeriodicSignal1 Property#
The source signal for the selected trigger is set to Periodic Signal 1.
Applies to: CamEmu and ace 2 GigE
PLCamera.TriggerSourceEnum.ShaftEncoderModuleOut Property#
The source signal for the selected trigger is set to the shaft encoder module.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Software Property#
The source signal for the selected trigger is set to software triggering.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.TriggerSourceEnum.SoftwareSignal1 Property#
The source signal for the selected trigger is set to software signal 1.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.SoftwareSignal2 Property#
The source signal for the selected trigger is set to software signal 2.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.SoftwareSignal3 Property#
The source signal for the selected trigger is set to software signal 3.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Timer1Active Property#
The Timer 1 Active trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Timer1End Property#
The Timer 1 End trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Timer1Start Property#
This enumeration value sets the signal source for the selected trigger to timer 1 start.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.Timer2Active Property#
The Timer 2 Active trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.Timer2End Property#
The Timer 2 End trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSourceEnum.UserOutput1 Property#
This enumeration value sets the signal source for the selected trigger to user output 1.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.UserOutput2 Property#
This enumeration value sets the signal source for the selected trigger to user output 2.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.VInput1 Property#
Sets the signal source for the selected trigger to Virtual Input 1.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.VInput2 Property#
Sets the signal source for the selected trigger to Virtual Input 2.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.VInput3 Property#
Sets the signal source for the selected trigger to Virtual Input 3.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.VInput4 Property#
Sets the signal source for the selected trigger to Virtual Input 4.
Applies to: CameraLink and GigE
PLCamera.TriggerSourceEnum.VInputDecActive Property#
Sets the signal source for the selected trigger to Virtual Input Decoder Active.
Applies to: CameraLink and GigE