pylon C++ Programmer's Guide#
はじめに#
プログラマーガイド | The pylon Programmer's Guide is a quick guide on how to program using the Basler pylon C++ API. It can can be used together with the pylon sample code for getting started. |
高度なトピック | The Advanced Topics section can be consulted if more information about special use cases is required. |
APIリファレンス | The API Reference provides documentation about the Basler pylon C++ interface. |
以前のバージョンからの移行 | The programming interface for pylon 6 is in some respects not backwards compatible with earlier versions. The migration guide describes the modifications needed to rebuild an application that was developed with earlier pylon versions. |
サンプルコード | The pylon sample code illustrates the common use cases when working with the pylon C++ API. |
ソフトウェアライセンスおよび法的情報 |
注意事項#
Caution:** The code snippets provided in this manual are included as sample code only. Inappropriate code may cause your camera to function differently than expected and may compromise your application. To ensure that the snippets will work properly in your application, you must adjust them to meet your specific needs and must test them thoroughly prior to use.
Parameter Reference#
pylon provides programming interface classes that are created from parameter description files. The table below links directly to the documentation of the generated classes.
All (Universal) | カメラ | Chunk Data | Event Grabber | Stream Grabber | トランスポート層 |
Other | Image Format Converter | Instant Camera | Video Writer | インターフェース |