PLTransportLayer.AreaTriggerModeEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.AreaTriggerModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.AreaTriggerModeEnum | Initializes a new instance of the PLTransportLayer.AreaTriggerModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
External | The trigger mode is set to External. Applies to: CoaXPress | |
Generator | The trigger mode is set to Generator. Applies to: CoaXPress | |
名前 | The full name of AreaTriggerMode (Overrides ParameterListEnum.Name.) | |
ソフトウェア | The trigger mode is set to Software. Applies to: CoaXPress | |
Synchronized | The trigger mode is set to Synchronized. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of AreaTriggerMode (Overrides Object.ToString()()()().) |
PLTransportLayer.AreaTriggerModeEnum.ToString Method#
The full name of AreaTriggerMode
Return Value#
Type: String
Returns the full name of AreaTriggerMode
PLTransportLayer.AreaTriggerModeEnum Constructor#
Initializes a new instance of the PLTransportLayer.AreaTriggerModeEnum class
PLTransportLayer.AreaTriggerModeEnum.External Property#
The trigger mode is set to External.
Applies to: CoaXPress
PLTransportLayer.AreaTriggerModeEnum.Generator Property#
The trigger mode is set to Generator.
Applies to: CoaXPress
PLTransportLayer.AreaTriggerModeEnum.Name Property#
The full name of AreaTriggerMode
PLTransportLayer.AreaTriggerModeEnum.Software Property#
The trigger mode is set to Software.
Applies to: CoaXPress
PLTransportLayer.AreaTriggerModeEnum.Synchronized Property#
The trigger mode is set to Synchronized.
Applies to: CoaXPress