PLCamera.SequenceControlSelectorEnum Class#
Applies to: CameraLink and GigE
Visibility: Guru
Selecting Parameters: SequenceControlSource
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.SequenceControlSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.SequenceControlSelectorEnum | Initializes a new instance of the PLCamera.SequenceControlSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Advance | The sequence set advance can be configured. Only available in Controlled sequence advance mode. Applies to: CameraLink and GigE | |
名前 | The full name of SequenceControlSelector (Overrides ParameterListEnum.Name.) | |
Restart | The sequence set restart can be configured. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of SequenceControlSelector (Overrides Object.ToString()()()().) |
PLCamera.SequenceControlSelectorEnum.ToString Method#
The full name of SequenceControlSelector
Return Value#
Type: String
Returns the full name of SequenceControlSelector
PLCamera.SequenceControlSelectorEnum Constructor#
Initializes a new instance of the PLCamera.SequenceControlSelectorEnum class
PLCamera.SequenceControlSelectorEnum.Advance Property#
The sequence set advance can be configured. Only available in Controlled sequence advance mode.
Applies to: CameraLink and GigE
PLCamera.SequenceControlSelectorEnum.Name Property#
The full name of SequenceControlSelector
PLCamera.SequenceControlSelectorEnum.Restart Property#
The sequence set restart can be configured.
Applies to: CameraLink and GigE