PLCamera.GevStreamChannelSelectorEnum Class#
Applies to: GigE
Visibility: Guru
Selecting Parameters: GevGVSPExtendedIDMode, GevSCBWA, GevSCBWR, GevSCBWRA, GevSCDA, GevSCDCT, GevSCDMT, GevSCFJM, GevSCFTD, GevSCPD, GevSCPHostPort, GevSCPInterfaceIndex, GevSCPSBigEndian, GevSCPSDoNotFragment, GevSCPSFireTestPacket, GevSCPSPacketSize
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.GevStreamChannelSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.GevStreamChannelSelectorEnum | Initializes a new instance of the PLCamera.GevStreamChannelSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of GevStreamChannelSelector (Overrides ParameterListEnum.Name.) | |
StreamChannel0 | Stream channel 0 can be configured. Applies to: GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of GevStreamChannelSelector (Overrides Object.ToString()()()().) |
PLCamera.GevStreamChannelSelectorEnum.ToString Method#
The full name of GevStreamChannelSelector
Return Value#
Type: String
Returns the full name of GevStreamChannelSelector
PLCamera.GevStreamChannelSelectorEnum Constructor#
Initializes a new instance of the PLCamera.GevStreamChannelSelectorEnum class
PLCamera.GevStreamChannelSelectorEnum.Name Property#
The full name of GevStreamChannelSelector
PLCamera.GevStreamChannelSelectorEnum.StreamChannel0 Property#
Stream channel 0 can be configured.
Applies to: GigE