Basler Vision Connector Messaging: Saving the Camera Configuration
With the GenICam protocol you can store parameter sets on the camera, and with the Basler Vision Connector you can save, load, and define the default user set to be used on camera restart.
After the camera has been parametrized, you can save the current parameters in a user set. To save the configuration, send the SaveUserSet
message.
JSON Payload
Field | Optional | タイプ | 説明 |
TransactionID | はい | String | Transaction identification |
アクション | いいえ | String | Method called. Fixed value: SaveUserSet |
DeviceID | いいえ | String | Device identification |
UserSet | いいえ | String/ Integer (64-bit signed) | {Value} or {IntValue} of the User Set Object as defined in Retrieving Available User Sets |
{
"TransactionID": "489494",
"Action": "SaveUserSet",
"DeviceID": "548451842342387",
"UserSet": "UserSet2"
}
Response Object
Field | Optional | タイプ | 説明 |
TransactionID | はい | String | Transaction identification |
ReturnCode | いいえ | Integer (32-bit unsigned) | Message code following Message Codes |
メッセージ | はい | String | Response message |
{
"TransactionID": "489494",
"ReturnCode": 0,
"Message": "User set updated."
}