PLTransportLayer.EventSelectorEnum Class#
Applies to: CoaXPress and blaze
Visibility: Expert
Selecting Parameters: EventNotification
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.EventSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.EventSelectorEnum | Initializes a new instance of the PLTransportLayer.EventSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AcquisitionTrigger | Entry for the event AcquisitionTrigger Applies to: CoaXPress | |
DeviceLost | The Device Lost event is selected. Applies to: CoaXPress and blaze | |
FrameTransferEnd | Entry for the event FrameTransferEnd Applies to: CoaXPress | |
FrameTransferStart | Entry for the event FrameTransferStart Applies to: CoaXPress | |
FrameTriggerMissed | Entry for the event FrameTriggerMissed Applies to: CoaXPress | |
名前 | The full name of EventSelector (Overrides ParameterListEnum.Name.) | |
Overflow | Entry for the event Overflow Applies to: CoaXPress | |
TriggerExceededPeriodLimits | Entry for the event TriggerExceededPeriodLimits Applies to: CoaXPress | |
TriggerQueueFilllevelThresholdOff | Entry for the event TriggerQueueFilllevelThresholdOff Applies to: CoaXPress | |
TriggerQueueFilllevelThresholdOn | Entry for the event TriggerQueueFilllevelThresholdOn Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of EventSelector (Overrides Object.ToString()()()().) |
PLTransportLayer.EventSelectorEnum.ToString Method#
The full name of EventSelector
Return Value#
Type: String
Returns the full name of EventSelector
PLTransportLayer.EventSelectorEnum Constructor#
Initializes a new instance of the PLTransportLayer.EventSelectorEnum class
PLTransportLayer.EventSelectorEnum.AcquisitionTrigger Property#
Entry for the event AcquisitionTrigger
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.DeviceLost Property#
The Device Lost event is selected.
Applies to: CoaXPress and blaze
PLTransportLayer.EventSelectorEnum.FrameTransferEnd Property#
Entry for the event FrameTransferEnd
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.FrameTransferStart Property#
Entry for the event FrameTransferStart
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.FrameTriggerMissed Property#
Entry for the event FrameTriggerMissed
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.Name Property#
The full name of EventSelector
PLTransportLayer.EventSelectorEnum.Overflow Property#
Entry for the event Overflow
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.TriggerExceededPeriodLimits Property#
Entry for the event TriggerExceededPeriodLimits
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.TriggerQueueFilllevelThresholdOff Property#
Entry for the event TriggerQueueFilllevelThresholdOff
Applies to: CoaXPress
PLTransportLayer.EventSelectorEnum.TriggerQueueFilllevelThresholdOn Property#
Entry for the event TriggerQueueFilllevelThresholdOn
Applies to: CoaXPress