PLCamera.BinningHorizontalModeEnum Class#
Applies to: CamEmu, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Expert
Selected by: BinningSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BinningHorizontalModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BinningHorizontalModeEnum | Initializes a new instance of the PLCamera.BinningHorizontalModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Average | The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light. Applies to: CamEmu, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
名前 | The full name of BinningHorizontalMode (Overrides ParameterListEnum.Name.) | |
Sum | The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio. Applies to: CamEmu, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BinningHorizontalMode (Overrides Object.ToString()()()().) |
PLCamera.BinningHorizontalModeEnum.ToString Method#
The full name of BinningHorizontalMode
Return Value#
Type: String
Returns the full name of BinningHorizontalMode
PLCamera.BinningHorizontalModeEnum Constructor#
Initializes a new instance of the PLCamera.BinningHorizontalModeEnum class
PLCamera.BinningHorizontalModeEnum.Average Property#
The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light.
Applies to: CamEmu, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.BinningHorizontalModeEnum.Name Property#
The full name of BinningHorizontalMode
PLCamera.BinningHorizontalModeEnum.Sum Property#
The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio.
Applies to: CamEmu, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB