PLCamera.BinningSelectorEnum Class#
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
Visibility: Expert
Selecting Parameters: BinningHorizontal, BinningHorizontalMode, BinningVertical, BinningVerticalMode
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BinningSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BinningSelectorEnum | Initializes a new instance of the PLCamera.BinningSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of BinningSelector (Overrides ParameterListEnum.Name.) | |
Region1 | FPGA binning can be configured. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
Sensor | Sensor binning can be configured. Applies to: boost CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BinningSelector (Overrides Object.ToString()()()().) |
PLCamera.BinningSelectorEnum.ToString Method#
The full name of BinningSelector
Return Value#
Type: String
Returns the full name of BinningSelector
PLCamera.BinningSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BinningSelectorEnum class
PLCamera.BinningSelectorEnum.Name Property#
The full name of BinningSelector
PLCamera.BinningSelectorEnum.Region1 Property#
FPGA binning can be configured.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.BinningSelectorEnum.Sensor Property#
Sensor binning can be configured.
Applies to: boost CoaXPress