PLCamera.UserSetDefaultEnum Class#
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.UserSetDefaultEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.UserSetDefaultEnum | Initializes a new instance of the PLCamera.UserSetDefaultEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AutoFunctions | The Auto Functions factory set is set as the default startup set. Applies to: ace USB | |
カラー | The factory set enabling color adjustments is set as the startup set. Applies to: ace USB | |
ColorRaw | The Color Raw factory set is set as the default startup set. Applies to: ace USB | |
Default | The Default User Set factory set is set as the default startup set. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
HighGain | The High Gain factory set is set as the default startup set. Applies to: ace USB | |
LightMicroscopy | The Light Microscopy factory set is set as the default startup set. Applies to: ace USB | |
名前 | The full name of UserSetDefault (Overrides ParameterListEnum.Name.) | |
UserSet1 | User set 1 is set as the default startup set. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
UserSet2 | User set 2 is set as the default startup set. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
UserSet3 | User set 3 is set as the default startup set. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of UserSetDefault (Overrides Object.ToString()()()().) |
PLCamera.UserSetDefaultEnum.ToString Method#
The full name of UserSetDefault
Return Value#
Type: String
Returns the full name of UserSetDefault
PLCamera.UserSetDefaultEnum Constructor#
Initializes a new instance of the PLCamera.UserSetDefaultEnum class
PLCamera.UserSetDefaultEnum.AutoFunctions Property#
The Auto Functions factory set is set as the default startup set.
Applies to: ace USB
PLCamera.UserSetDefaultEnum.Color Property#
The factory set enabling color adjustments is set as the startup set.
Applies to: ace USB
PLCamera.UserSetDefaultEnum.ColorRaw Property#
The Color Raw factory set is set as the default startup set.
Applies to: ace USB
PLCamera.UserSetDefaultEnum.Default Property#
The Default User Set factory set is set as the default startup set.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.UserSetDefaultEnum.HighGain Property#
The High Gain factory set is set as the default startup set.
Applies to: ace USB
PLCamera.UserSetDefaultEnum.LightMicroscopy Property#
The Light Microscopy factory set is set as the default startup set.
Applies to: ace USB
PLCamera.UserSetDefaultEnum.Name Property#
The full name of UserSetDefault
PLCamera.UserSetDefaultEnum.UserSet1 Property#
User set 1 is set as the default startup set.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.UserSetDefaultEnum.UserSet2 Property#
User set 2 is set as the default startup set.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.UserSetDefaultEnum.UserSet3 Property#
User set 3 is set as the default startup set.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB