Basler _UniversalEventParams#
クラス#
名前 | |
---|---|
class | Basler_UniversalEventParams::CUniversalEventParams_Params A parameter class containing all parameters as members that are available for pylon event grabbers. |
class | Basler_UniversalEventParams::CUniversalEventParams_Params_v7_4_0 A parameter class containing all parameters as members that are available for pylon event grabbers. |
タイプ#
名前 | |
---|---|
enum | StatusEnums { Status_Closed, Status_Open} Valid values for Status. |
Types Documentation#
enum StatusEnums#
Enumerator | 値 | 説明 |
---|---|---|
Status_Closed | The low level event grabber is closed - Applies to: GigE. | |
Status_Open | The low level event grabber is open - Applies to: GigE. |