PLCamera.TriggerSelectorEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
Selected by: TriggerControlImplementation
Selecting Parameters: TriggerActivation, TriggerDelay, TriggerDelayAbs, TriggerDelayLineTriggerCount, TriggerDelaySource, TriggerMode, TriggerPartialClosingFrame, TriggerSoftware, TriggerSource
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TriggerSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.TriggerSelectorEnum | Initializes a new instance of the PLCamera.TriggerSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AcquisitionActive | This enumeration value selects the acquisition active trigger for configuration. Applies to: CameraLink and GigE | |
AcquisitionEnd | This enumeration value selects the acquisition end trigger for configuration. Applies to: CameraLink and GigE | |
AcquisitionStart | The Acquisition Start trigger can be configured. Applies to: CameraLink and GigE | |
ExposureActive | The Exposure Active trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
ExposureEnd | The Exposure End trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
ExposureStart | The Exposure Start trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
FrameActive | The Frame Active trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstActive | The Frame Burst Active trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstEnd | The Frame Burst End trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstStart | The Frame Burst Start trigger can be configured. Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
FrameEnd | The Frame End trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameStart | The Frame Start trigger can be configured. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
LineStart | The Line Start trigger can be configured. Applies to: CameraLink and GigE | |
名前 | The full name of TriggerSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerSelector (Overrides Object.ToString()()()().) |
PLCamera.TriggerSelectorEnum.ToString Method#
The full name of TriggerSelector
Return Value#
Type: String
Returns the full name of TriggerSelector
PLCamera.TriggerSelectorEnum Constructor#
Initializes a new instance of the PLCamera.TriggerSelectorEnum class
PLCamera.TriggerSelectorEnum.AcquisitionActive Property#
This enumeration value selects the acquisition active trigger for configuration.
Applies to: CameraLink and GigE
PLCamera.TriggerSelectorEnum.AcquisitionEnd Property#
This enumeration value selects the acquisition end trigger for configuration.
Applies to: CameraLink and GigE
PLCamera.TriggerSelectorEnum.AcquisitionStart Property#
The Acquisition Start trigger can be configured.
Applies to: CameraLink and GigE
PLCamera.TriggerSelectorEnum.ExposureActive Property#
The Exposure Active trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.ExposureEnd Property#
The Exposure End trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.ExposureStart Property#
The Exposure Start trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.FrameActive Property#
The Frame Active trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.FrameBurstActive Property#
The Frame Burst Active trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.FrameBurstEnd Property#
The Frame Burst End trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.FrameBurstStart Property#
The Frame Burst Start trigger can be configured.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.FrameEnd Property#
The Frame End trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TriggerSelectorEnum.FrameStart Property#
The Frame Start trigger can be configured.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.TriggerSelectorEnum.LineStart Property#
The Line Start trigger can be configured.
Applies to: CameraLink and GigE
PLCamera.TriggerSelectorEnum.Name Property#
The full name of TriggerSelector