GenICam#
クラス#
名前 | |
---|---|
class | GenICam::gcstring A string class which is a clone of std::string. |
Functions#
名前 | |
---|---|
std::istream & | getline(std::istream & is, GenICam::gcstring & str) |
std::istream & | getline(std::istream & is, GenICam::gcstring & str, char delim) |
Detailed Description#
Contains definitions of GenICam types and exceptions.
GenICam is an alias for a more complex namespace name, e.g. GenICam_3_1_Basler_pylon. Throughout this documentation, only the alias GenICam is used. When programming applications using pylon, we also recommend to only use the Pylon and the GenApi namespaces. Most of the types in the GenICam namespace can also be found in the Pylon namespace. You should use Pylon::String_t instead of GenICam::gcstring and Pylon::GenericException instead of GenICam::GenericException. The latter applies to all exceptions in the GenICam namespace.
Functions Documentation#
function getline#
STL getline
function getline#
STL getline