PLCamera.ShadingSetSelectorEnum Class#
Applies to: CameraLink and GigE
Visibility: Expert
Selected by: ShadingSelector
Selecting Parameters: ShadingSetActivate, ShadingSetCreate
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ShadingSetSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ShadingSetSelectorEnum | Initializes a new instance of the PLCamera.ShadingSetSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
DefaultShadingSet | The default shading set can be loaded using the Activate command. Applies to: CameraLink and GigE | |
名前 | The full name of ShadingSetSelector (Overrides ParameterListEnum.Name.) | |
UserShadingSet1 | User Shading Set 1 can be loaded using the Activate command. Applies to: CameraLink and GigE | |
UserShadingSet2 | User Shading Set 2 can be loaded using the Activate command. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ShadingSetSelector (Overrides Object.ToString()()()().) |
PLCamera.ShadingSetSelectorEnum.ToString Method#
The full name of ShadingSetSelector
Return Value#
Type: String
Returns the full name of ShadingSetSelector
PLCamera.ShadingSetSelectorEnum Constructor#
Initializes a new instance of the PLCamera.ShadingSetSelectorEnum class
PLCamera.ShadingSetSelectorEnum.DefaultShadingSet Property#
The default shading set can be loaded using the Activate command.
Applies to: CameraLink and GigE
PLCamera.ShadingSetSelectorEnum.Name Property#
The full name of ShadingSetSelector
PLCamera.ShadingSetSelectorEnum.UserShadingSet1 Property#
User Shading Set 1 can be loaded using the Activate command.
Applies to: CameraLink and GigE
PLCamera.ShadingSetSelectorEnum.UserShadingSet2 Property#
User Shading Set 2 can be loaded using the Activate command.
Applies to: CameraLink and GigE