PLCamera.SequenceAddressBitSelectorEnum Class#
Applies to: CameraLink and GigE
Visibility: Guru
Selecting Parameters: SequenceAddressBitSource
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.SequenceAddressBitSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.SequenceAddressBitSelectorEnum | Initializes a new instance of the PLCamera.SequenceAddressBitSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Bit0 | Bit 0 of the sequence set address can be controlled using an input line. Applies to: CameraLink and GigE | |
Bit1 | Bit 1 of the sequence set address can be controlled using an input line. Applies to: CameraLink and GigE | |
Bit2 | Bit 2 of the sequence set address can be controlled using an input line. Applies to: CameraLink and GigE | |
Bit3 | Bit 3 of the sequence set address can be controlled using an input line. Applies to: CameraLink and GigE | |
名前 | The full name of SequenceAddressBitSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of SequenceAddressBitSelector (Overrides Object.ToString()()()().) |
PLCamera.SequenceAddressBitSelectorEnum.ToString Method#
The full name of SequenceAddressBitSelector
Return Value#
Type: String
Returns the full name of SequenceAddressBitSelector
PLCamera.SequenceAddressBitSelectorEnum Constructor#
Initializes a new instance of the PLCamera.SequenceAddressBitSelectorEnum class
PLCamera.SequenceAddressBitSelectorEnum.Bit0 Property#
Bit 0 of the sequence set address can be controlled using an input line.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSelectorEnum.Bit1 Property#
Bit 1 of the sequence set address can be controlled using an input line.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSelectorEnum.Bit2 Property#
Bit 2 of the sequence set address can be controlled using an input line.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSelectorEnum.Bit3 Property#
Bit 3 of the sequence set address can be controlled using an input line.
Applies to: CameraLink and GigE
PLCamera.SequenceAddressBitSelectorEnum.Name Property#
The full name of SequenceAddressBitSelector