PLCamera.BLCSerialPortBaudRateEnum Class#
Applies to: GigE and ace USB
Visibility: Guru
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BLCSerialPortBaudRateEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BLCSerialPortBaudRateEnum | Initializes a new instance of the PLCamera.BLCSerialPortBaudRateEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Baud115200 | The baud rate is 115200 Bd. Applies to: GigE and ace USB | |
名前 | The full name of BLCSerialPortBaudRate (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BLCSerialPortBaudRate (Overrides Object.ToString()()()().) |
PLCamera.BLCSerialPortBaudRateEnum.ToString Method#
The full name of BLCSerialPortBaudRate
Return Value#
Type: String
Returns the full name of BLCSerialPortBaudRate
PLCamera.BLCSerialPortBaudRateEnum Constructor#
Initializes a new instance of the PLCamera.BLCSerialPortBaudRateEnum class
PLCamera.BLCSerialPortBaudRateEnum.Baud115200 Property#
The baud rate is 115200 Bd.
Applies to: GigE and ace USB
PLCamera.BLCSerialPortBaudRateEnum.Name Property#
The full name of BLCSerialPortBaudRate