PLCamera.SensorReadoutModeEnum Class#
Applies to: GigE and ace USB
Visibility: Guru
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.SensorReadoutModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.SensorReadoutModeEnum | Initializes a new instance of the PLCamera.SensorReadoutModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Fast | The readout time for each row of pixels is reduced, compared to normal readout. This allows the the camera to operate at higher frame rates. This can, however, result in reduced image quality. Applies to: GigE and ace USB | |
名前 | The full name of SensorReadoutMode (Overrides ParameterListEnum.Name.) | |
Normal | The camera operates in normal readout mode. Applies to: GigE and ace USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of SensorReadoutMode (Overrides Object.ToString()()()().) |
PLCamera.SensorReadoutModeEnum.ToString Method#
The full name of SensorReadoutMode
Return Value#
Type: String
Returns the full name of SensorReadoutMode
PLCamera.SensorReadoutModeEnum Constructor#
Initializes a new instance of the PLCamera.SensorReadoutModeEnum class
PLCamera.SensorReadoutModeEnum.Fast Property#
The readout time for each row of pixels is reduced, compared to normal readout. This allows the the camera to operate at higher frame rates. This can, however, result in reduced image quality.
Applies to: GigE and ace USB
PLCamera.SensorReadoutModeEnum.Name Property#
The full name of SensorReadoutMode
PLCamera.SensorReadoutModeEnum.Normal Property#
The camera operates in normal readout mode.
Applies to: GigE and ace USB