PLCamera.LUTSelectorEnum Class#
Applies to: CameraLink, GigE and ace USB
Visibility: Beginner
Selecting Parameters: LUTEnable, LUTIndex, LUTValue, LUTValueAll
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.LUTSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.LUTSelectorEnum | Initializes a new instance of the PLCamera.LUTSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Luminance | The luminance lookup table can be configured. Applies to: CameraLink, GigE and ace USB | |
名前 | The full name of LUTSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of LUTSelector (Overrides Object.ToString()()()().) |
PLCamera.LUTSelectorEnum.ToString Method#
The full name of LUTSelector
Return Value#
Type: String
Returns the full name of LUTSelector
PLCamera.LUTSelectorEnum Constructor#
Initializes a new instance of the PLCamera.LUTSelectorEnum class
PLCamera.LUTSelectorEnum.Luminance Property#
The luminance lookup table can be configured.
Applies to: CameraLink, GigE and ace USB
PLCamera.LUTSelectorEnum.Name Property#
The full name of LUTSelector