PLCamera.SequenceConfigurationModeEnum Class#
Applies to: GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.SequenceConfigurationModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.SequenceConfigurationModeEnum | Initializes a new instance of the PLCamera.SequenceConfigurationModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of SequenceConfigurationMode (Overrides ParameterListEnum.Name.) | |
Off | The sequencer can't be configured. Applies to: GigE | |
その | The sequencer can be configured. Applies to: GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of SequenceConfigurationMode (Overrides Object.ToString()()()().) |
PLCamera.SequenceConfigurationModeEnum.ToString Method#
The full name of SequenceConfigurationMode
Return Value#
Type: String
Returns the full name of SequenceConfigurationMode
PLCamera.SequenceConfigurationModeEnum Constructor#
Initializes a new instance of the PLCamera.SequenceConfigurationModeEnum class
PLCamera.SequenceConfigurationModeEnum.Name Property#
The full name of SequenceConfigurationMode
PLCamera.SequenceConfigurationModeEnum.Off Property#
The sequencer can't be configured.
Applies to: GigE
PLCamera.SequenceConfigurationModeEnum.On Property#
The sequencer can be configured.
Applies to: GigE