低レベルAPI#
クラス#
名前 | |
---|---|
class | Pylon::CChunkParser Low Level API: Base class for chunk parsers returned by camera objects. |
class | Pylon::GrabResult Low Level API: A grab result that combines the used image buffer and status information. |
class | Pylon::EventResult Low Level API: An event result. |
class | Pylon::CGrabResultImageT Low Level API: Adapts grab result to Pylon::IImage. |
class | Pylon::CStreamGrabberProxyT Low Level API: The stream grabber class with parameter access methods. |
interface | Pylon::IChunkParser Low Level API: The interface for chunk parsers analyzing a data stream consisting of chunks. |
interface | Pylon::ISelfReliantChunkParser Low Level API: Interface for chunk parsers with an own chunk data node map attached. |
interface | Pylon::IDevice Low Level API: The interface implemented by all device objects. |
interface | Pylon::IPylonDevice Low Level API: Interface for camera objects. |
interface | Pylon::IEventAdapter Low Level API: IEventAdapter delivers event messages to ports. |
interface | Pylon::IEventGrabber Low Level API: Interface of an object receiving asynchronous events. |
interface | Pylon::IStreamGrabber Low Level API: Interface to an (input) data stream. |
interface | Pylon::IPylonGigEDevice Low Level API: The interface for Basler GigE camera devices. |
タイプ#
名前 | |
---|---|
enum | EGrabStatus { GrabStatus_Undefined = -1, _UndefinedGrabStatus = GrabStatus_Undefined, GrabStatus_Idle, Idle = GrabStatus_Idle, GrabStatus_Queued, Queued = GrabStatus_Queued, GrabStatus_Grabbed, Grabbed = GrabStatus_Grabbed, GrabStatus_Canceled, Canceled = GrabStatus_Canceled, GrabStatus_Failed, Failed = GrabStatus_Failed} Low Level API: Possible grab status values. |
typedef CGrabResultImageT< GrabResult > | CGrabResultImage Low Level API: Adapts a copy of a grab result to pylon image. |
Functions#
名前 | |
---|---|
template <class Function > DeviceCallbackHandle | RegisterRemovalCallback(IPylonDevice * pDevice, Function f) Low Level API: Register a C-function as a removal callback. |
template <class Client ,class Member > DeviceCallbackHandle | RegisterRemovalCallback(IPylonDevice * pDevice, Client & c, Member m) Low Level API: Register a C++-member function as removal callback. |
Types Documentation#
enum EGrabStatus#
Enumerator | 値 | 説明 |
---|---|---|
GrabStatus_Undefined | -1 | |
_UndefinedGrabStatus | GrabStatus_Undefined | |
GrabStatus_Idle | Currently not used. | |
Idle | GrabStatus_Idle | Currently not used. For backward compatibility only. |
GrabStatus_Queued | Grab request is in the input queue. | |
Queued | GrabStatus_Queued | Grab request is in the input queue. For backward compatibility only. Consider using GrabStatus_Queued instead. |
GrabStatus_Grabbed | Grab request terminated successfully. Buffer is filled with data. | |
Grabbed | GrabStatus_Grabbed | Grab request terminated successfully. Buffer is filled with data. For backward compatibility only. Consider using GrabStatus_Grabbed instead. |
GrabStatus_Canceled | Grab request was canceled. Buffer doesn't contain valid data. | |
Canceled | GrabStatus_Canceled | Grab request was canceled. Buffer doesn't contain valid data. For backward compatibility only. Consider using GrabStatus_Canceled instead. |
GrabStatus_Failed | Grab request failed. Buffer doesn't contain valid data. | |
Failed | GrabStatus_Failed | Grab request failed. Buffer doesn't contain valid data. For backward compatibility only. Consider using GrabStatus_Queued instead. |
Low Level API: Possible grab status values.
typedef CGrabResultImage#
Low Level API: Adapts a copy of a grab result to pylon image.
Attention: The referenced grab result must not be destroyed and the result's buffer must not be queued for grabbing again during the lifetime of this object.
Functions Documentation#
function RegisterRemovalCallback#
template <class Function >
DeviceCallbackHandle RegisterRemovalCallback(
IPylonDevice * pDevice,
Function f
)
Low Level API: Register a C-function as a removal callback.
Parameters:
- pDevice Pointer to the device that generates callbacks
- f The function to be called
See: Pylon::IPylonDevice::RegisterRemovalCallback()
function RegisterRemovalCallback#
template <class Client ,
class Member >
DeviceCallbackHandle RegisterRemovalCallback(
IPylonDevice * pDevice,
Client & c,
Member m
)
Low Level API: Register a C++-member function as removal callback.
Parameters:
- pDevice Pointer to the device that generates callbacks
- c The client object
- m The member function to be called