PLCamera.BslMultipleROIRowSelectorEnum Class#
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
Visibility: Expert
Selecting Parameters: BslMultipleROIRowOffset, BslMultipleROIRowSize
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslMultipleROIRowSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslMultipleROIRowSelectorEnum | Initializes a new instance of the PLCamera.BslMultipleROIRowSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of BslMultipleROIRowSelector (Overrides ParameterListEnum.Name.) | |
Row1 | Row 1 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row10 | Row 10 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row11 | Row 11 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row12 | Row 12 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row13 | Row 13 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row14 | Row 14 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row15 | Row 15 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row16 | Row 16 can be configured. Applies to: ace 2 GigE and ace 2 USB | |
Row2 | Row 2 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row3 | Row 3 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row4 | Row 4 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row5 | Row 5 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row6 | Row 6 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row7 | Row 7 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row8 | Row 8 can be configured. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Row9 | Row 9 can be configured. Applies to: ace 2 GigE and ace 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslMultipleROIRowSelector (Overrides Object.ToString()()()().) |
PLCamera.BslMultipleROIRowSelectorEnum.ToString Method#
The full name of BslMultipleROIRowSelector
Return Value#
Type: String
Returns the full name of BslMultipleROIRowSelector
PLCamera.BslMultipleROIRowSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BslMultipleROIRowSelectorEnum class
PLCamera.BslMultipleROIRowSelectorEnum.Name Property#
The full name of BslMultipleROIRowSelector
PLCamera.BslMultipleROIRowSelectorEnum.Row1 Property#
Row 1 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row10 Property#
Row 10 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row11 Property#
Row 11 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row12 Property#
Row 12 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row13 Property#
Row 13 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row14 Property#
Row 14 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row15 Property#
Row 15 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row16 Property#
Row 16 can be configured.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.BslMultipleROIRowSelectorEnum.Row2 Property#
Row 2 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row3 Property#
Row 3 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row4 Property#
Row 4 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row5 Property#
Row 5 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row6 Property#
Row 6 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row7 Property#
Row 7 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row8 Property#
Row 8 can be configured.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslMultipleROIRowSelectorEnum.Row9 Property#
Row 9 can be configured.
Applies to: ace 2 GigE and ace 2 USB