PLCamera.ClPixelClockEnum Class#
Applies to: CameraLink
Visibility: Guru
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ClPixelClockEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ClPixelClockEnum | Initializes a new instance of the PLCamera.ClPixelClockEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of ClPixelClock (Overrides ParameterListEnum.Name.) | |
PixelClock20 | The pixel clock speed is set to 20 MHz. Applies to: CameraLink | |
PixelClock32_5 | The pixel clock speed is set to 32.5 MHz. Applies to: CameraLink | |
PixelClock40 | The pixel clock speed is set to 40 MHz. Applies to: CameraLink | |
PixelClock48 | The pixel clock speed is set to 48 MHz. Applies to: CameraLink | |
PixelClock65 | The pixel clock speed is set to 65 MHz. Applies to: CameraLink | |
PixelClock82 | The pixel clock speed is set to 82 MHz. Applies to: CameraLink | |
PixelClock82_5 | The pixel clock speed is set to 82.5 MHz. Applies to: CameraLink | |
PixelClock83 | The pixel clock speed is set to 83 MHz. Applies to: CameraLink | |
PixelClock83_5 | The pixel clock speed is set to 83.5 MHz. Applies to: CameraLink |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ClPixelClock (Overrides Object.ToString()()()().) |
PLCamera.ClPixelClockEnum.ToString Method#
The full name of ClPixelClock
Return Value#
Type: String
Returns the full name of ClPixelClock
PLCamera.ClPixelClockEnum Constructor#
Initializes a new instance of the PLCamera.ClPixelClockEnum class
PLCamera.ClPixelClockEnum.Name Property#
The full name of ClPixelClock
PLCamera.ClPixelClockEnum.PixelClock20 Property#
The pixel clock speed is set to 20 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock32_5 Property#
The pixel clock speed is set to 32.5 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock40 Property#
The pixel clock speed is set to 40 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock48 Property#
The pixel clock speed is set to 48 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock65 Property#
The pixel clock speed is set to 65 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock82 Property#
The pixel clock speed is set to 82 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock82_5 Property#
The pixel clock speed is set to 82.5 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock83 Property#
The pixel clock speed is set to 83 MHz.
Applies to: CameraLink
PLCamera.ClPixelClockEnum.PixelClock83_5 Property#
The pixel clock speed is set to 83.5 MHz.
Applies to: CameraLink