PLCamera.ShaftEncoderModuleModeEnum Class#
Applies to: CameraLink and GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ShaftEncoderModuleModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ShaftEncoderModuleModeEnum | Initializes a new instance of the PLCamera.ShaftEncoderModuleModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AnyDirection | The shaft encoder module outputs trigger signals for forward and reverse ticks, provided the reverse counter is neither increasing nor decreasing. Applies to: CameraLink and GigE | |
ForwardOnly | The shaft encoder module outputs trigger signals for forward ticks only, provided the reverse counter is neither increasing nor decreasing. Applies to: CameraLink and GigE | |
名前 | The full name of ShaftEncoderModuleMode (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ShaftEncoderModuleMode (Overrides Object.ToString()()()().) |
PLCamera.ShaftEncoderModuleModeEnum.ToString Method#
The full name of ShaftEncoderModuleMode
Return Value#
Type: String
Returns the full name of ShaftEncoderModuleMode
PLCamera.ShaftEncoderModuleModeEnum Constructor#
Initializes a new instance of the PLCamera.ShaftEncoderModuleModeEnum class
PLCamera.ShaftEncoderModuleModeEnum.AnyDirection Property#
The shaft encoder module outputs trigger signals for forward and reverse ticks, provided the reverse counter is neither increasing nor decreasing.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleModeEnum.ForwardOnly Property#
The shaft encoder module outputs trigger signals for forward ticks only, provided the reverse counter is neither increasing nor decreasing.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleModeEnum.Name Property#
The full name of ShaftEncoderModuleMode