PLTransportLayer.TriggerStateEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerStateEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.TriggerStateEnum | Initializes a new instance of the PLTransportLayer.TriggerStateEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Active | The trigger state is set to Active. In this state, the trigger system is fully enabled. Applies to: CoaXPress | |
AsyncStop | The trigger state is set to AsyncStop. This state asynchronously and immediately stops the trigger system. Note that this may result in output signals of undefined signal length as a current signal generation might be interrupted. Restarting a previously stopped trigger, i.e., switching to the 'Active' state, will clear the queue and the sequencer. Applies to: CoaXPress | |
名前 | The full name of TriggerState (Overrides ParameterListEnum.Name.) | |
SyncStop | The trigger state is set to SyncStop. In this state, the trigger system ignores further input pulses or stops the generation of pulses. Pulses currently in the system will still be processed, however. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerState (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerStateEnum.ToString Method#
The full name of TriggerState
Return Value#
Type: String
Returns the full name of TriggerState
PLTransportLayer.TriggerStateEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerStateEnum class
PLTransportLayer.TriggerStateEnum.Active Property#
The trigger state is set to Active. In this state, the trigger system is fully enabled.
Applies to: CoaXPress
PLTransportLayer.TriggerStateEnum.AsyncStop Property#
The trigger state is set to AsyncStop. This state asynchronously and immediately stops the trigger system. Note that this may result in output signals of undefined signal length as a current signal generation might be interrupted. Restarting a previously stopped trigger, i.e., switching to the 'Active' state, will clear the queue and the sequencer.
Applies to: CoaXPress
PLTransportLayer.TriggerStateEnum.Name Property#
The full name of TriggerState
PLTransportLayer.TriggerStateEnum.SyncStop Property#
The trigger state is set to SyncStop. In this state, the trigger system ignores further input pulses or stops the generation of pulses. Pulses currently in the system will still be processed, however.
Applies to: CoaXPress