PLCamera.EventSelectorEnum Class#
Applies to: GigE, ace 2 GigE, ace 2 USB, ace USB and dart 2 USB
Visibility: Beginner
Selecting Parameters: EventNotification
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.EventSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.EventSelectorEnum | Initializes a new instance of the PLCamera.EventSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AcquisitionStart | Event notifications for the Acquisition Start event can be enabled. An Acquisition Start event is raised whenever the Acquisition Start trigger is activated. It is not associated with the Acquisition Start command. Applies to: GigE | |
AcquisitionStartOvertrigger | Event notifications for the Acquisition Start Overtrigger event can be enabled. Applies to: GigE | |
AcquisitionStartWait | Event notifications for the Acquisition Start Wait event can be enabled. Applies to: GigE | |
AcquisitionWait | Event notifications for the Acquisition Wait event can be enabled. Applies to: GigE | |
ActionLate | Event notifications for the Action Late event can be enabled. Applies to: GigE and ace 2 GigE | |
CriticalTemperature | Event notifications for the Critical Temperature event can be enabled. Applies to: GigE and ace USB | |
EventOverrun | Event notifications for the Event Overrun event can be enabled. Applies to: GigE | |
ExposureEnd | Event notifications for the Exposure End event can be enabled. Applies to: GigE, ace 2 GigE, ace 2 USB, ace USB and dart 2 USB | |
FrameBufferOverrun | Event notifications for the Frame Buffer Overrun event can be enabled. Applies to: ace 2 GigE and ace 2 USB | |
FrameBurstStart | Event notifications for the Frame Burst Start event can be enabled. Applies to: ace USB | |
FrameBurstStartOvertrigger | Event notifications for the Frame Burst Start Overtrigger event can be enabled. Applies to: ace USB | |
FrameBurstStartWait | Event notifications for the Frame Burst Start Wait event can be enabled. Applies to: ace USB | |
FrameStart | Event notifications for the Frame Start event can be enabled. Applies to: GigE, ace 2 GigE, ace 2 USB, ace USB and dart 2 USB | |
FrameStartOvertrigger | Event notifications for the Frame Start Overtrigger event can be enabled. Applies to: GigE and ace USB | |
FrameStartWait | Event notifications for the Frame Start Wait event can be enabled. Applies to: GigE and ace USB | |
FrameTimeout | Event notifications for the Frame Timeout event can be enabled. Applies to: GigE | |
FrameTriggerMissed | Event notifications for the Frame Trigger Missed event can be enabled. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
FrameWait | Event notifications for the Frame Wait event can be enabled. Applies to: GigE | |
Line1RisingEdge | The event will be generated when a Rising Edge is detected on the Line 1 Applies to: GigE | |
Line2RisingEdge | The event will be generated when a Rising Edge is detected on the Line 2 Applies to: GigE | |
Line3RisingEdge | The event will be generated when a Rising Edge is detected on the Line 3 Applies to: GigE | |
Line4RisingEdge | The event will be generated when a Rising Edge is detected on the Line 4 Applies to: GigE | |
LineStartOvertrigger | Event notifications for the Line Start Overtrigger event can be enabled. Applies to: GigE | |
名前 | The full name of EventSelector (Overrides ParameterListEnum.Name.) | |
Overrun | Event notifications for the Overrun event can be enabled. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
OverTemperature | Event notifications for the Over Temperature event can be enabled. Applies to: GigE and ace USB | |
TemperatureStatusChanged | Event notifications for the Temperature Status Changed event can be enabled. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
テスト | Event notifications for the Test event can be enabled. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
VirtualLine1RisingEdge | The event will be generated when a Rising Edge is detected on the Virtual Line 1 Applies to: GigE | |
VirtualLine2RisingEdge | The event will be generated when a Rising Edge is detected on the Virtual Line 2 Applies to: GigE | |
VirtualLine3RisingEdge | The event will be generated when a Rising Edge is detected on the Virtual Line 3 Applies to: GigE | |
VirtualLine4RisingEdge | The event will be generated when a Rising Edge is detected on the Virtual Line 4 Applies to: GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of EventSelector (Overrides Object.ToString()()()().) |
PLCamera.EventSelectorEnum.ToString Method#
The full name of EventSelector
Return Value#
Type: String
Returns the full name of EventSelector
PLCamera.EventSelectorEnum Constructor#
Initializes a new instance of the PLCamera.EventSelectorEnum class
PLCamera.EventSelectorEnum.AcquisitionStart Property#
Event notifications for the Acquisition Start event can be enabled. An Acquisition Start event is raised whenever the Acquisition Start trigger is activated. It is not associated with the Acquisition Start command.
Applies to: GigE
PLCamera.EventSelectorEnum.AcquisitionStartOvertrigger Property#
Event notifications for the Acquisition Start Overtrigger event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.AcquisitionStartWait Property#
Event notifications for the Acquisition Start Wait event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.AcquisitionWait Property#
Event notifications for the Acquisition Wait event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.ActionLate Property#
Event notifications for the Action Late event can be enabled.
Applies to: GigE and ace 2 GigE
PLCamera.EventSelectorEnum.CriticalTemperature Property#
Event notifications for the Critical Temperature event can be enabled.
Applies to: GigE and ace USB
PLCamera.EventSelectorEnum.EventOverrun Property#
Event notifications for the Event Overrun event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.ExposureEnd Property#
Event notifications for the Exposure End event can be enabled.
Applies to: GigE, ace 2 GigE, ace 2 USB, ace USB and dart 2 USB
PLCamera.EventSelectorEnum.FrameBufferOverrun Property#
Event notifications for the Frame Buffer Overrun event can be enabled.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.EventSelectorEnum.FrameBurstStart Property#
Event notifications for the Frame Burst Start event can be enabled.
Applies to: ace USB
PLCamera.EventSelectorEnum.FrameBurstStartOvertrigger Property#
Event notifications for the Frame Burst Start Overtrigger event can be enabled.
Applies to: ace USB
PLCamera.EventSelectorEnum.FrameBurstStartWait Property#
Event notifications for the Frame Burst Start Wait event can be enabled.
Applies to: ace USB
PLCamera.EventSelectorEnum.FrameStart Property#
Event notifications for the Frame Start event can be enabled.
Applies to: GigE, ace 2 GigE, ace 2 USB, ace USB and dart 2 USB
PLCamera.EventSelectorEnum.FrameStartOvertrigger Property#
Event notifications for the Frame Start Overtrigger event can be enabled.
Applies to: GigE and ace USB
PLCamera.EventSelectorEnum.FrameStartWait Property#
Event notifications for the Frame Start Wait event can be enabled.
Applies to: GigE and ace USB
PLCamera.EventSelectorEnum.FrameTimeout Property#
Event notifications for the Frame Timeout event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.FrameTriggerMissed Property#
Event notifications for the Frame Trigger Missed event can be enabled.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.EventSelectorEnum.FrameWait Property#
Event notifications for the Frame Wait event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.Line1RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Line 1
Applies to: GigE
PLCamera.EventSelectorEnum.Line2RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Line 2
Applies to: GigE
PLCamera.EventSelectorEnum.Line3RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Line 3
Applies to: GigE
PLCamera.EventSelectorEnum.Line4RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Line 4
Applies to: GigE
PLCamera.EventSelectorEnum.LineStartOvertrigger Property#
Event notifications for the Line Start Overtrigger event can be enabled.
Applies to: GigE
PLCamera.EventSelectorEnum.Name Property#
The full name of EventSelector
PLCamera.EventSelectorEnum.Overrun Property#
Event notifications for the Overrun event can be enabled.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.EventSelectorEnum.OverTemperature Property#
Event notifications for the Over Temperature event can be enabled.
Applies to: GigE and ace USB
PLCamera.EventSelectorEnum.TemperatureStatusChanged Property#
Event notifications for the Temperature Status Changed event can be enabled.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.EventSelectorEnum.Test Property#
Event notifications for the Test event can be enabled.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.EventSelectorEnum.VirtualLine1RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Virtual Line 1
Applies to: GigE
PLCamera.EventSelectorEnum.VirtualLine2RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Virtual Line 2
Applies to: GigE
PLCamera.EventSelectorEnum.VirtualLine3RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Virtual Line 3
Applies to: GigE
PLCamera.EventSelectorEnum.VirtualLine4RisingEdge Property#
The event will be generated when a Rising Edge is detected on the Virtual Line 4
Applies to: GigE