PLCamera.CxpSendReceiveSelectorEnum Class#
Applies to: boost CoaXPress and boost_V_CoaXPress
Visibility: Expert
Selected by: CxpConnectionSelector
Selecting Parameters: CxpConnectionTestPacketCount
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpSendReceiveSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.CxpSendReceiveSelectorEnum | Initializes a new instance of the PLCamera.CxpSendReceiveSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of CxpSendReceiveSelector (Overrides ParameterListEnum.Name.) | |
Receive | The receive features can be configured. Applies to: boost CoaXPress and boost_V_CoaXPress | |
送信 | The send features can be configured. Applies to: boost CoaXPress and boost_V_CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of CxpSendReceiveSelector (Overrides Object.ToString()()()().) |
PLCamera.CxpSendReceiveSelectorEnum.ToString Method#
The full name of CxpSendReceiveSelector
Return Value#
Type: String
Returns the full name of CxpSendReceiveSelector
PLCamera.CxpSendReceiveSelectorEnum Constructor#
Initializes a new instance of the PLCamera.CxpSendReceiveSelectorEnum class
PLCamera.CxpSendReceiveSelectorEnum.Name Property#
The full name of CxpSendReceiveSelector
PLCamera.CxpSendReceiveSelectorEnum.Receive Property#
The receive features can be configured.
Applies to: boost CoaXPress and boost_V_CoaXPress
PLCamera.CxpSendReceiveSelectorEnum.Send Property#
The send features can be configured.
Applies to: boost CoaXPress and boost_V_CoaXPress