PLTransportLayer.SystemmonitorPowerOverCxpStateEnum Class#
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.SystemmonitorPowerOverCxpStateEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum | Initializes a new instance of the PLTransportLayer.SystemmonitorPowerOverCxpStateEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of SystemmonitorPowerOverCxpState (Overrides ParameterListEnum.Name.) | |
PoCXPADCChipError | ADC Chip Error Applies to: CoaXPress | |
PoCXPBooting | Booting, not initalized Applies to: CoaXPress | |
PoCXPDisabled | No Power over CXP Applies to: CoaXPress | |
PoCXPLowVolt | Low voltage Applies to: CoaXPress | |
PoCXPMaxCurrent | Maximum current Applies to: CoaXPress | |
PoCXPMinCurrent | Minimum current Applies to: CoaXPress | |
PoCXPNotConnected | No cable connected Applies to: CoaXPress | |
PoCXPOK | Power over CXP OK Applies to: CoaXPress | |
PoCXPOverVolt | Over voltage Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of SystemmonitorPowerOverCxpState (Overrides Object.ToString()()()().) |
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.ToString Method#
The full name of SystemmonitorPowerOverCxpState
Return Value#
Type: String
Returns the full name of SystemmonitorPowerOverCxpState
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum Constructor#
Initializes a new instance of the PLTransportLayer.SystemmonitorPowerOverCxpStateEnum class
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.Name Property#
The full name of SystemmonitorPowerOverCxpState
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPADCChipError Property#
ADC Chip Error
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPBooting Property#
Booting, not initalized
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPDisabled Property#
No Power over CXP
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPLowVolt Property#
Low voltage
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPMaxCurrent Property#
Maximum current
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPMinCurrent Property#
Minimum current
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPNotConnected Property#
No cable connected
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPOK Property#
Power over CXP OK
Applies to: CoaXPress
PLTransportLayer.SystemmonitorPowerOverCxpStateEnum.PoCXPOverVolt Property#
Over voltage
Applies to: CoaXPress