PLCamera.UserSetSelectorEnum Class#
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
Selecting Parameters: UserSetLoad, UserSetSave
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.UserSetSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.UserSetSelectorEnum | Initializes a new instance of the PLCamera.UserSetSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AutoFunctions | The Auto Functions factory set can be loaded. This user set enables the camera's Exposure Auto and Gain Auto auto functions. Applies to: CameraLink, GigE and ace USB | |
カラー | The Color factory set can be loaded. This user set configures the camera to produce good color images under the most common lighting conditions. Applies to: CameraLink, GigE and ace USB | |
ColorRaw | The Color Raw factory set can be loaded. This user set disables the color enhancement features. Applies to: GigE and ace USB | |
Custom0 | The Custom 0 factory set can be loaded. Applies to: CameraLink and GigE | |
Custom1 | The Custom 1 factory set can be loaded. Applies to: CameraLink and GigE | |
Default | The Default User Set factory set can be loaded. This user set configures the camera to provide good camera performance in many common applications under normal conditions. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
HighGain | The High Gain factory set can be loaded. This user set increases the gain by 6 dB. Applies to: CameraLink, GigE and ace USB | |
LightMicroscopy | The Light Microscopy factory set can be loaded. Applies to: GigE and ace USB | |
名前 | The full name of UserSetSelector (Overrides ParameterListEnum.Name.) | |
UserSet1 | User set 1 can be saved, loaded, or configured. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
UserSet2 | User set 2 can be saved, loaded, or configured. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
UserSet3 | User set 3 can be saved, loaded, or configured. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of UserSetSelector (Overrides Object.ToString()()()().) |
PLCamera.UserSetSelectorEnum.ToString Method#
The full name of UserSetSelector
Return Value#
Type: String
Returns the full name of UserSetSelector
PLCamera.UserSetSelectorEnum Constructor#
Initializes a new instance of the PLCamera.UserSetSelectorEnum class
PLCamera.UserSetSelectorEnum.AutoFunctions Property#
The Auto Functions factory set can be loaded. This user set enables the camera's Exposure Auto and Gain Auto auto functions.
Applies to: CameraLink, GigE and ace USB
PLCamera.UserSetSelectorEnum.Color Property#
The Color factory set can be loaded. This user set configures the camera to produce good color images under the most common lighting conditions.
Applies to: CameraLink, GigE and ace USB
PLCamera.UserSetSelectorEnum.ColorRaw Property#
The Color Raw factory set can be loaded. This user set disables the color enhancement features.
Applies to: GigE and ace USB
PLCamera.UserSetSelectorEnum.Custom0 Property#
The Custom 0 factory set can be loaded.
Applies to: CameraLink and GigE
PLCamera.UserSetSelectorEnum.Custom1 Property#
The Custom 1 factory set can be loaded.
Applies to: CameraLink and GigE
PLCamera.UserSetSelectorEnum.Default Property#
The Default User Set factory set can be loaded. This user set configures the camera to provide good camera performance in many common applications under normal conditions.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.UserSetSelectorEnum.HighGain Property#
The High Gain factory set can be loaded. This user set increases the gain by 6 dB.
Applies to: CameraLink, GigE and ace USB
PLCamera.UserSetSelectorEnum.LightMicroscopy Property#
The Light Microscopy factory set can be loaded.
Applies to: GigE and ace USB
PLCamera.UserSetSelectorEnum.Name Property#
The full name of UserSetSelector
PLCamera.UserSetSelectorEnum.UserSet1 Property#
User set 1 can be saved, loaded, or configured.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.UserSetSelectorEnum.UserSet2 Property#
User set 2 can be saved, loaded, or configured.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.UserSetSelectorEnum.UserSet3 Property#
User set 3 can be saved, loaded, or configured.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB