PLCamera.AutoFunctionAOISelectorEnum Class#
Applies to: CameraLink and GigE
Visibility: Beginner
Selecting Parameters: AutoFunctionAOIHeight, AutoFunctionAOIOffsetX, AutoFunctionAOIOffsetY, AutoFunctionAOIUsageIntensity, AutoFunctionAOIUsageRedLightCorrection, AutoFunctionAOIUsageWhiteBalance, AutoFunctionAOIWidth
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.AutoFunctionAOISelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.AutoFunctionAOISelectorEnum | Initializes a new instance of the PLCamera.AutoFunctionAOISelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AOI1 | Auto function AOI 1 can be configured. Applies to: CameraLink and GigE | |
AOI2 | Auto function AOI 2 can be configured. Applies to: CameraLink and GigE | |
AOI3 | Applies to: CameraLink and GigE | |
AOI4 | Applies to: CameraLink and GigE | |
AOI5 | Applies to: CameraLink and GigE | |
AOI6 | Applies to: CameraLink and GigE | |
AOI7 | Applies to: CameraLink and GigE | |
AOI8 | Applies to: CameraLink and GigE | |
名前 | The full name of AutoFunctionAOISelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of AutoFunctionAOISelector (Overrides Object.ToString()()()().) |
PLCamera.AutoFunctionAOISelectorEnum.ToString Method#
The full name of AutoFunctionAOISelector
Return Value#
Type: String
Returns the full name of AutoFunctionAOISelector
PLCamera.AutoFunctionAOISelectorEnum Constructor#
Initializes a new instance of the PLCamera.AutoFunctionAOISelectorEnum class
PLCamera.AutoFunctionAOISelectorEnum.AOI1 Property#
Auto function AOI 1 can be configured.
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI2 Property#
Auto function AOI 2 can be configured.
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI3 Property#
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI4 Property#
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI5 Property#
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI6 Property#
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI7 Property#
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.AOI8 Property#
Applies to: CameraLink and GigE
PLCamera.AutoFunctionAOISelectorEnum.Name Property#
The full name of AutoFunctionAOISelector