PLCamera.ShaftEncoderModuleLineSourceEnum Class#
Applies to: CameraLink and GigE
Visibility: Expert
Selected by: ShaftEncoderModuleLineSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ShaftEncoderModuleLineSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ShaftEncoderModuleLineSourceEnum | Initializes a new instance of the PLCamera.ShaftEncoderModuleLineSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
CC1 | The source signal for the shaft encoder module is set to CC1. Applies to: CameraLink and GigE | |
CC2 | The source signal for the shaft encoder module is set to CC2. Applies to: CameraLink and GigE | |
CC3 | The source signal for the shaft encoder module is set to CC3. Applies to: CameraLink and GigE | |
CC4 | The source signal for the shaft encoder module is set to CC4. Applies to: CameraLink and GigE | |
Line1 | The source signal for the shaft encoder module is set to input line 1. Applies to: CameraLink and GigE | |
Line2 | The source signal for the shaft encoder module is set to input line 2. Applies to: CameraLink and GigE | |
Line3 | The source signal for the shaft encoder module is set to input line 3. Applies to: CameraLink and GigE | |
Line4 | The source signal for the shaft encoder module is set to input line 4. Applies to: CameraLink and GigE | |
Line5 | This enumeration value selects input line 5 as signal source for the shaft encoder module. Applies to: CameraLink and GigE | |
Line6 | This enumeration value selects input line 6 as signal source for the shaft encoder module. Applies to: CameraLink and GigE | |
Line7 | This enumeration value selects input line 7 as signal source for the shaft encoder module. Applies to: CameraLink and GigE | |
Line8 | This enumeration value selects input line 8 as signal source for the shaft encoder module. Applies to: CameraLink and GigE | |
名前 | The full name of ShaftEncoderModuleLineSource (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ShaftEncoderModuleLineSource (Overrides Object.ToString()()()().) |
PLCamera.ShaftEncoderModuleLineSourceEnum.ToString Method#
The full name of ShaftEncoderModuleLineSource
Return Value#
Type: String
Returns the full name of ShaftEncoderModuleLineSource
PLCamera.ShaftEncoderModuleLineSourceEnum Constructor#
Initializes a new instance of the PLCamera.ShaftEncoderModuleLineSourceEnum class
PLCamera.ShaftEncoderModuleLineSourceEnum.CC1 Property#
The source signal for the shaft encoder module is set to CC1.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.CC2 Property#
The source signal for the shaft encoder module is set to CC2.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.CC3 Property#
The source signal for the shaft encoder module is set to CC3.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.CC4 Property#
The source signal for the shaft encoder module is set to CC4.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line1 Property#
The source signal for the shaft encoder module is set to input line 1.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line2 Property#
The source signal for the shaft encoder module is set to input line 2.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line3 Property#
The source signal for the shaft encoder module is set to input line 3.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line4 Property#
The source signal for the shaft encoder module is set to input line 4.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line5 Property#
This enumeration value selects input line 5 as signal source for the shaft encoder module.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line6 Property#
This enumeration value selects input line 6 as signal source for the shaft encoder module.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line7 Property#
This enumeration value selects input line 7 as signal source for the shaft encoder module.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Line8 Property#
This enumeration value selects input line 8 as signal source for the shaft encoder module.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleLineSourceEnum.Name Property#
The full name of ShaftEncoderModuleLineSource