PLCamera.IntensityCalculationEnum Class#
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.IntensityCalculationEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.IntensityCalculationEnum | Initializes a new instance of the PLCamera.IntensityCalculationEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Method1 | Method 1 is used to calculate the intensity image. This is the default value. In scenes containing motion, you may notice a lag between the depth image and the intensity image. Applies to: blaze | |
Method2 | Method 2 is used to calculate the intensity image. This ensures that the depth image and the intensity image are in synch. The disadvantage is that the resulting intensity image will be darker and contain more noise. Applies to: blaze | |
名前 | The full name of IntensityCalculation (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of IntensityCalculation (Overrides Object.ToString()()()().) |
PLCamera.IntensityCalculationEnum.ToString Method#
The full name of IntensityCalculation
Return Value#
Type: String
Returns the full name of IntensityCalculation
PLCamera.IntensityCalculationEnum Constructor#
Initializes a new instance of the PLCamera.IntensityCalculationEnum class
PLCamera.IntensityCalculationEnum.Method1 Property#
Method 1 is used to calculate the intensity image. This is the default value. In scenes containing motion, you may notice a lag between the depth image and the intensity image.
Applies to: blaze
PLCamera.IntensityCalculationEnum.Method2 Property#
Method 2 is used to calculate the intensity image. This ensures that the depth image and the intensity image are in synch. The disadvantage is that the resulting intensity image will be darker and contain more noise.
Applies to: blaze
PLCamera.IntensityCalculationEnum.Name Property#
The full name of IntensityCalculation