PLCamera.BslChunkTimestampSelectorEnum Class#
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
Visibility: Expert
Selecting Parameters: BslChunkTimestampValue
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslChunkTimestampSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslChunkTimestampSelectorEnum | Initializes a new instance of the PLCamera.BslChunkTimestampSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
ExposureEnd | The Chunk Timestamp Value parameter indicates when exposure of the current image ended. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
ExposureStart | The Chunk Timestamp Value parameter indicates when exposure of the current image started. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
FrameStart | The Chunk Timestamp Value parameter indicates when acquisition of the current image started. Applies to: ace 2 GigE, ace 2 USB and dart 2 USB | |
名前 | The full name of BslChunkTimestampSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslChunkTimestampSelector (Overrides Object.ToString()()()().) |
PLCamera.BslChunkTimestampSelectorEnum.ToString Method#
The full name of BslChunkTimestampSelector
Return Value#
Type: String
Returns the full name of BslChunkTimestampSelector
PLCamera.BslChunkTimestampSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BslChunkTimestampSelectorEnum class
PLCamera.BslChunkTimestampSelectorEnum.ExposureEnd Property#
The Chunk Timestamp Value parameter indicates when exposure of the current image ended.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.BslChunkTimestampSelectorEnum.ExposureStart Property#
The Chunk Timestamp Value parameter indicates when exposure of the current image started.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.BslChunkTimestampSelectorEnum.FrameStart Property#
The Chunk Timestamp Value parameter indicates when acquisition of the current image started.
Applies to: ace 2 GigE, ace 2 USB and dart 2 USB
PLCamera.BslChunkTimestampSelectorEnum.Name Property#
The full name of BslChunkTimestampSelector