PLCamera.BslLightControlSourceEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightControlSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslLightControlSourceEnum | Initializes a new instance of the PLCamera.BslLightControlSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Line3 | Line 3 is used to control the light features. Applies to: GigE and ace USB | |
Line4 | Line 4 is used to control the light features. Applies to: GigE and ace USB | |
名前 | The full name of BslLightControlSource (Overrides ParameterListEnum.Name.) | |
Off | No line is used to control the light features. Applies to: GigE and ace USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslLightControlSource (Overrides Object.ToString()()()().) |
PLCamera.BslLightControlSourceEnum.ToString Method#
The full name of BslLightControlSource
Return Value#
Type: String
Returns the full name of BslLightControlSource
PLCamera.BslLightControlSourceEnum Constructor#
Initializes a new instance of the PLCamera.BslLightControlSourceEnum class
PLCamera.BslLightControlSourceEnum.Line3 Property#
Line 3 is used to control the light features.
Applies to: GigE and ace USB
PLCamera.BslLightControlSourceEnum.Line4 Property#
Line 4 is used to control the light features.
Applies to: GigE and ace USB
PLCamera.BslLightControlSourceEnum.Name Property#
The full name of BslLightControlSource
PLCamera.BslLightControlSourceEnum.Off Property#
No line is used to control the light features.
Applies to: GigE and ace USB