GenApiインターフェース#
タイプ#
名前 | |
---|---|
enum | EGenApiAccessMode { NI, NA, WO, RO, RW, _UndefinedAccesMode = -1} Access mode of a node. |
enum | EGenApiCachingMode { NoCache, WriteThrough, WriteAround, _UndefinedCachingMode = -1} Node caching modes. |
enum | EGenApiFileAccessMode { GenApiFileReadAccess, GenApiFileWriteAccess} File access modes. |
enum | EGenApiNameSpace { Custom, Standard, _UndefinedNameSpace = -1} Node name spaces. |
enum | EGenApiNodeType { IntegerNode, BooleanNode, FloatNode, CommandNode, StringNode, EnumerationNode, EnumEntryNode, Category, _UnknownNodeType = -1} Node type. |
enum | EGenApiRepresentation { Linear, Logarithmic, Boolean, PureNumber, HexNumber, _UndefinedRepresentation = -1} Node representation. |
enum | EGenApiVisibility { Beginner = 0, Expert = 1, Guru = 2, Invisible = 3, _UndefinedVisibility = -1} Node visibility. |
typedef struct GENAPI_FILE_HANDLE_ * | GENAPI_FILE_HANDLE A handle for a GenApi file object. |
typedef struct NODE_CALLBACK_HANDLE_ * | NODE_CALLBACK_HANDLE A handle for a node callback object. |
typedef struct NODE_HANDLE_ * | NODE_HANDLE A handle for a node object. |
typedef struct NODEMAP_HANDLE_ * | NODEMAP_HANDLE A handle for a node map object. |
Functions#
名前 | |
---|---|
GENAPIC_RESULT | GenApiBooleanGetValue(NODE_HANDLE hNode, _Bool * pValue) Return a node's boolean value. |
GENAPIC_RESULT | GenApiBooleanSetValue(NODE_HANDLE hNode, _Bool value) Set a node's boolean value. |
GENAPIC_RESULT | GenApiCategoryGetFeatureByIndex(NODE_HANDLE hNode, size_t index, NODE_HANDLE * phEntry) Get a feature node from a category by its index. |
GENAPIC_RESULT | GenApiCategoryGetNumFeatures(NODE_HANDLE hNode, size_t * pValue) Returns the number of features in a category. |
GENAPIC_RESULT | GenApiCommandExecute(NODE_HANDLE hNode) Trigger the execution of a command. |
GENAPIC_RESULT | GenApiCommandIsDone(NODE_HANDLE hNode, _Bool * pValue) Check whether command has finished. |
GENAPIC_RESULT | GenApiEnumerationEntryGetSymbolic(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return the symbolic name of an enumeration entry node. |
GENAPIC_RESULT | GenApiEnumerationEntryGetValue(NODE_HANDLE hNode, int * pValue) Returns the numerical index of an enumeration entry. |
GENAPIC_RESULT | GenApiEnumerationGetEntryByIndex(NODE_HANDLE hNode, size_t index, NODE_HANDLE * pEntry) Get an entry from an enumeration by index. |
GENAPIC_RESULT | GenApiEnumerationGetEntryByName(NODE_HANDLE hNode, const char * pName, NODE_HANDLE * pEntry) Get an entry from an enumeration by name. |
GENAPIC_RESULT | GenApiEnumerationGetNumEntries(NODE_HANDLE hNode, size_t * pValue) Get the number of entries in an enumeration. |
GENAPIC_RESULT | GenApiFileClose(GENAPI_FILE_HANDLE hFile) Closes a file. |
GENAPIC_RESULT | GenApiFileExists(NODEMAP_HANDLE hMap, const char * pFileName, _Bool * pResult) Check whether a file exists. |
GENAPIC_RESULT | GenApiFileOpen(NODEMAP_HANDLE hMap, const char * pFileName, EGenApiFileAccessMode accessMode, GENAPI_FILE_HANDLE * phFile) Opens a file. |
GENAPIC_RESULT | GenApiFileRead(GENAPI_FILE_HANDLE hFile, void * pBuffer, size_t * pLength) Reads binary data from a file. |
GENAPIC_RESULT | GenApiFilesAreSupported(NODEMAP_HANDLE hMap, _Bool * pResult) Check whether the device supports accessing files. |
GENAPIC_RESULT | GenApiFileWrite(GENAPI_FILE_HANDLE hFile, const void * pBuffer, size_t length) Writes binary data to a file. |
GENAPIC_RESULT | GenApiFloatGetMax(NODE_HANDLE hNode, double * pValue) Get a node's maximum floating-point value. |
GENAPIC_RESULT | GenApiFloatGetMin(NODE_HANDLE hNode, double * pValue) Get a node's minimum floating-point value. |
GENAPIC_RESULT | GenApiFloatGetRepresentation(NODE_HANDLE hNode, EGenApiRepresentation * pValue) Get a node's preferred representation. |
GENAPIC_RESULT | GenApiFloatGetUnit(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return a floating-point node's unit. |
GENAPIC_RESULT | GenApiFloatGetValue(NODE_HANDLE hNode, double * pValue) Get a node's floating-point value without validation. |
GENAPIC_RESULT | GenApiFloatGetValueEx(NODE_HANDLE hNode, _Bool verify, double * pValue) Return a node's floating-point value with optional validation. |
GENAPIC_RESULT | GenApiFloatSetValue(NODE_HANDLE hNode, double value) Set a node's floating-point value with mandatory validation. |
GENAPIC_RESULT | GenApiFloatSetValueEx(NODE_HANDLE hNode, _Bool verify, double value) Set a node's floating-point value with optional validation. |
GENAPIC_RESULT | GenApiGetLastErrorDetail(char * pBuf, size_t * pBufLen) Get detailed textual description for the latest error details, e.g. the origin of the error. |
GENAPIC_RESULT | GenApiGetLastErrorMessage(char * pBuf, size_t * pBufLen) Get a brief textual description of the latest error. |
GENAPIC_RESULT | GenApiIntegerGetInc(NODE_HANDLE hNode, int64_t * pValue) Get the value increment from an integer node. |
GENAPIC_RESULT | GenApiIntegerGetIncInt32(NODE_HANDLE hNode, int32_t * pValue) Get the value increment from an integer node. |
GENAPIC_RESULT | GenApiIntegerGetMax(NODE_HANDLE hNode, int64_t * pValue) Get the maximum value from an integer node. |
GENAPIC_RESULT | GenApiIntegerGetMaxInt32(NODE_HANDLE hNode, int32_t * pValue) Get the maximum value from an integer node. |
GENAPIC_RESULT | GenApiIntegerGetMin(NODE_HANDLE hNode, int64_t * pValue) Get the minimum value from an integer node. |
GENAPIC_RESULT | GenApiIntegerGetMinInt32(NODE_HANDLE hNode, int32_t * pValue) Get the minimum value from an integer node. |
GENAPIC_RESULT | GenApiIntegerGetRepresentation(NODE_HANDLE hNode, EGenApiRepresentation * pValue) Get a node's preferred representation. |
GENAPIC_RESULT | GenApiIntegerGetValue(NODE_HANDLE hNode, int64_t * pValue) Get a node's integer value without validation. |
GENAPIC_RESULT | GenApiIntegerGetValueEx(NODE_HANDLE hNode, _Bool verify, int64_t * pValue) Return a node's integer value with optional validation. |
GENAPIC_RESULT | GenApiIntegerGetValueExInt32(NODE_HANDLE hNode, _Bool verify, int32_t * pValue) Return a node's integer value with optional validation. |
GENAPIC_RESULT | GenApiIntegerGetValueInt32(NODE_HANDLE hNode, int32_t * pValue) Get a node's integer value without validation. |
GENAPIC_RESULT | GenApiIntegerSetValue(NODE_HANDLE hNode, int64_t value) Set a node's integer value with mandatory validation. |
GENAPIC_RESULT | GenApiIntegerSetValueEx(NODE_HANDLE hNode, _Bool verify, int64_t value) Set a node's integer value with optional validation. |
GENAPIC_RESULT | GenApiIntegerSetValueExInt32(NODE_HANDLE hNode, _Bool verify, int32_t value) Set a node's integer value with optional validation. |
GENAPIC_RESULT | GenApiIntegerSetValueInt32(NODE_HANDLE hNode, int32_t value) Set a node's integer value with mandatory validation. |
GENAPIC_RESULT | GenApiNodeDeregisterCallback(NODE_HANDLE hNode, NODE_CALLBACK_HANDLE hCb) Remove a node callback function. |
GENAPIC_RESULT | GenApiNodeFromString(NODE_HANDLE hNode, const char * pString) Set a node's value from a text string with mandatory validation. |
GENAPIC_RESULT | GenApiNodeFromStringEx(NODE_HANDLE hNode, _Bool verify, const char * pString) Set a node's value from a text string with optional validation. |
GENAPIC_RESULT | GenApiNodeGetAccessMode(NODE_HANDLE hNode, EGenApiAccessMode * pAccessMode) Query node for allowed access modes. |
GENAPIC_RESULT | GenApiNodeGetAlias(NODE_HANDLE hNode, NODE_HANDLE * phNode) Get a node's alias. |
GENAPIC_RESULT | GenApiNodeGetCachingMode(NODE_HANDLE hNode, EGenApiCachingMode * pCachingMode) Query node for its caching mode. |
GENAPIC_RESULT | GenApiNodeGetDescription(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return a node's description text. |
GENAPIC_RESULT | GenApiNodeGetDisplayName(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return a node's user-friendly name. |
GENAPIC_RESULT | GenApiNodeGetName(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return a node's name. |
GENAPIC_RESULT | GenApiNodeGetNameSpace(NODE_HANDLE hNode, EGenApiNameSpace * pNamespace) Return a node's name space. |
GENAPIC_RESULT | GenApiNodeGetPollingTime(NODE_HANDLE hNode, int64_t * pPollingTime) Query a node for its recommended polling interval. |
GENAPIC_RESULT | GenApiNodeGetPollingTimeInt32(NODE_HANDLE hNode, int32_t * pPollingTime) Query a node for its recommended polling interval. |
GENAPIC_RESULT | GenApiNodeGetToolTip(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return a node's tool tip text. |
GENAPIC_RESULT | GenApiNodeGetType(NODE_HANDLE hNode, EGenApiNodeType * pType) Get node type. |
GENAPIC_RESULT | GenApiNodeGetVisibility(NODE_HANDLE hNode, EGenApiVisibility * pVisibility) Return a node's visibility. |
GENAPIC_RESULT | GenApiNodeImposeAccessMode(NODE_HANDLE hNode, EGenApiAccessMode imposedAccessMode) Modify a node's accessibility. |
GENAPIC_RESULT | GenApiNodeImposeVisibility(NODE_HANDLE hNode, EGenApiVisibility imposedVisibility) Modify a node's visibility. |
GENAPIC_RESULT | GenApiNodeInvalidateNode(NODE_HANDLE hNode) Mark node as possibly changed. |
GENAPIC_RESULT | GenApiNodeIsAvailable(NODE_HANDLE hNode, _Bool * pResult) Check whether a feature's value is available. |
GENAPIC_RESULT | GenApiNodeIsImplemented(NODE_HANDLE hNode, _Bool * pResult) Check whether a feature is implemented. |
GENAPIC_RESULT | GenApiNodeIsReadable(NODE_HANDLE hNode, _Bool * pResult) Check whether a feature's value is readable. |
GENAPIC_RESULT | GenApiNodeIsWritable(NODE_HANDLE hNode, _Bool * pResult) Check whether a feature's value is writable. |
GENAPIC_RESULT | GenApiNodeMapGetNode(NODEMAP_HANDLE hMap, const char * pName, NODE_HANDLE * phNode) Find a node by its name. |
GENAPIC_RESULT | GenApiNodeMapGetNodeByIndex(NODEMAP_HANDLE hMap, size_t index, NODE_HANDLE * phNode) Find a node by its index. |
GENAPIC_RESULT | GenApiNodeMapGetNumNodes(NODEMAP_HANDLE hMap, size_t * pValue) Get the number of nodes contained in a node map. |
GENAPIC_RESULT | GenApiNodeMapPoll(NODEMAP_HANDLE hMap, int64_t timestamp) Poll all nodes in a node map. |
GENAPIC_RESULT | GenApiNodeMapPollInt32(NODEMAP_HANDLE hMap, int32_t timestamp) Poll all nodes in a node map. |
GENAPIC_RESULT | GenApiNodeRegisterCallback(NODE_HANDLE hNode, NodeCallbackFunction_t * pCbFunction, NODE_CALLBACK_HANDLE * phCb) Install a node callback function. |
GENAPIC_RESULT | GenApiNodeToString(NODE_HANDLE hNode, char * pBuf, size_t * pBufLen) Return a textual representation of a node's value. |
GENAPIC_RESULT | GenApiNodeToStringEx(NODE_HANDLE hNode, _Bool verify, char * pBuf, size_t * pBufLen) Return a textual representation of a node's value with optional validation. |
GENAPIC_RESULT | GenApiPortRead(NODE_HANDLE hNode, void * pBuffer, int64_t Address, size_t Length) Perform a raw read on the port implemented by the node passed. |
GENAPIC_RESULT | GenApiPortWrite(NODE_HANDLE hNode, const void * pBuffer, int64_t Address, size_t Length) Perform a raw write on the port implemented by the node passed. |
GENAPIC_RESULT | GenApiRegisterGetAddress(NODE_HANDLE hNode, int64_t * pAddress) Returns the address of the register node. |
GENAPIC_RESULT | GenApiRegisterGetLength(NODE_HANDLE hNode, size_t * pLength) Returns the length in bytes of the register node. |
GENAPIC_RESULT | GenApiRegisterGetValue(NODE_HANDLE hNode, void * pBuffer, size_t * pLength) Reads binary data from the register node. |
GENAPIC_RESULT | GenApiRegisterSetValue(NODE_HANDLE hNode, const void * pBuffer, size_t length) Writes binary data to the register node. |
GENAPIC_RESULT | GenApiSelectorGetNumSelectedFeatures(NODE_HANDLE hNode, size_t * pValue) Return the number of selected nodes. |
GENAPIC_RESULT | GenApiSelectorGetNumSelectingFeatures(NODE_HANDLE hNode, size_t * pValue) Return the number of selecting features. |
GENAPIC_RESULT | GenApiSelectorGetSelectedFeatureByIndex(NODE_HANDLE hNode, size_t index, NODE_HANDLE * phNode) Get a selected node by its index. |
GENAPIC_RESULT | GenApiSelectorGetSelectingFeatureByIndex(NODE_HANDLE hNode, size_t index, NODE_HANDLE * phNode) Return a selecting feature by its index. |
Defines#
名前 |
---|
GENAPIC_INVALID_HANDLE A value for invalid / uninitialized handles. |
Types Documentation#
enum EGenApiAccessMode#
Enumerator | 値 | 説明 |
---|---|---|
NI | Not implemented. | |
NA | Not available. | |
WO | Write Only. | |
RO | Read Only. | |
RW | Read and Write. | |
_UndefinedAccesMode | -1 | Access mode invalid. |
enum EGenApiCachingMode#
Enumerator | 値 | 説明 |
---|---|---|
NoCache | Do not use cache. | |
WriteThrough | Write to cache and register. | |
WriteAround | Write to register, write to cache on read. | |
_UndefinedCachingMode | -1 | Caching mode invalid. |
Node caching modes.
enum EGenApiFileAccessMode#
Enumerator | 値 | 説明 |
---|---|---|
GenApiFileReadAccess | For specifying file read access on file open. | |
GenApiFileWriteAccess | For specifying file write access on file open. |
File access modes.
enum EGenApiNameSpace#
Enumerator | 値 | 説明 |
---|---|---|
Custom | Name resides in custom name space. | |
Standard | Name resides in one of the standard name spaces. | |
_UndefinedNameSpace | -1 | Name space invalid. |
Node name spaces.
enum EGenApiNodeType#
Enumerator | 値 | 説明 |
---|---|---|
IntegerNode | Node represents an integer-valued parameter. | |
BooleanNode | Node represents a boolean (true/false) parameter. | |
FloatNode | Node represents a floating point-valued parameter. | |
CommandNode | Node can trigger a command. | |
StringNode | Node represents a string-valued parameter. | |
EnumerationNode | Node represents an enumeration-valued parameter. | |
EnumEntryNode | Node represents an 'enumeration entry' parameter. | |
Category | Node for grouping parameters in a category. | |
_UnknownNodeType | -1 | Node type invalid. |
Node type.
enum EGenApiRepresentation#
Enumerator | 値 | 説明 |
---|---|---|
Linear | Slider with linear behavior. | |
Logarithmic | Slider with logarithmic behavior. | |
Boolean | Checkbox. | |
PureNumber | Decimal number in an edit control. | |
HexNumber | Hex number in an edit control. | |
_UndefinedRepresentation | -1 | Representation invalid. |
Node representation.
enum EGenApiVisibility#
Enumerator | 値 | 説明 |
---|---|---|
Beginner | 0 | Visible to everyone. |
Expert | 1 | Visible to experts or gurus only. |
Guru | 2 | Visible to gurus only. |
Invisible | 3 | Not visible at all. |
_UndefinedVisibility | -1 | Visibility invalid. |
Node visibility.
typedef GENAPI_FILE_HANDLE#
A handle for a GenApi file object.
typedef NODE_CALLBACK_HANDLE#
A handle for a node callback object.
typedef NODE_HANDLE#
A handle for a node object.
typedef NODEMAP_HANDLE#
A handle for a node map object.
Functions Documentation#
function GenApiBooleanGetValue#
Return a node's boolean value.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Get the boolean value of a node. The function will fail if the node is of a type that has no such value.
function GenApiBooleanSetValue#
Set a node's boolean value.
Parameters:
- hNode Node to operate on
- value Boolean value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular boolean value. The function will fail if the node is of a type that has no such value.
function GenApiCategoryGetFeatureByIndex#
GENAPIC_RESULT GenApiCategoryGetFeatureByIndex(
NODE_HANDLE hNode,
size_t index,
NODE_HANDLE * phEntry
)
Get a feature node from a category by its index.
Parameters:
- hNode Category node handle
- index Index in category
- phEntry result node handle pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Returns a NODE_HANDLE for a feature node identified by its index. Using the value returned by GenApiCategoryGetNumFeatures(), this can be used to implement a loop to iterate over all feature nodes in a given category.
function GenApiCategoryGetNumFeatures#
Returns the number of features in a category.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the number of feature nodes that a category node manages.
function GenApiCommandExecute#
Trigger the execution of a command.
Parameters:
- hNode Node to operate on
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Execute the command associated with a command node.
function GenApiCommandIsDone#
Check whether command has finished.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
After initiating a command using GenApiCommandExecute(), use this function to check whether the command has run to completion.
function GenApiEnumerationEntryGetSymbolic#
GENAPIC_RESULT GenApiEnumerationEntryGetSymbolic(
NODE_HANDLE hNode,
char * pBuf,
size_t * pBufLen
)
Return the symbolic name of an enumeration entry node.
Parameters:
- hNode Node to operate on
- pBuf Pointer to user-supplied character buffer, or
NULL
- pBufLen Pointer to actual buffer size
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the symbolic name of an 'enumeration entry' node. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiEnumerationEntryGetValue#
Returns the numerical index of an enumeration entry.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the numerical index of an 'enumeration entry' node.
function GenApiEnumerationGetEntryByIndex#
GENAPIC_RESULT GenApiEnumerationGetEntryByIndex(
NODE_HANDLE hNode,
size_t index,
NODE_HANDLE * pEntry
)
Get an entry from an enumeration by index.
Parameters:
- hNode Node to operate on
- index Index of entry to get
- pEntry Pointer to variable receiving result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return a handle for an enumeration entry node identified by a numerical index. Using the number of entries returned by GenApiEnumerationGetNumEntries(), this can be used to iterate over every enumeration entry contained in an enumeration.
function GenApiEnumerationGetEntryByName#
GENAPIC_RESULT GenApiEnumerationGetEntryByName(
NODE_HANDLE hNode,
const char * pName,
NODE_HANDLE * pEntry
)
Get an entry from an enumeration by name.
Parameters:
- hNode Node to operate on
- pName Name of entry to get
- pEntry Pointer to variable receiving result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return a handle for an enumeration entry node identified by its name.
function GenApiEnumerationGetNumEntries#
Get the number of entries in an enumeration.
Parameters:
- hNode Node to operate on
- pValue Pointer to variable receiving result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Get the number of entries for an enumeration node.
function GenApiFileClose#
Closes a file.
Parameters:
- hFile The file handle.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Closes a file. The handle is invalid after closing.
function GenApiFileExists#
Check whether a file exists.
Parameters:
- hMap Device Node map handle.
- pFileName The name of the file.
- pResult Returns true if the file exists.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Check whether a file exists.
function GenApiFileOpen#
GENAPIC_RESULT GenApiFileOpen(
NODEMAP_HANDLE hMap,
const char * pFileName,
EGenApiFileAccessMode accessMode,
GENAPI_FILE_HANDLE * phFile
)
Opens a file.
Parameters:
- hMap Device Node map handle.
- pFileName The name of the file.
- accessMode Specifies read or write access.
- phFile Returns the file handle.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Only one file can be opened at a time per node map. The file is automatically closed if the node map is destroyed.
function GenApiFileRead#
Reads binary data from a file.
Parameters:
- hFile The file handle.
- pBuffer The data buffer.
- pLength Specifies the size of the buffer. Returns the count of bytes read.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
The end of file is reached if zero bytes are returned and the return error code is GENAPI_E_OK.
function GenApiFilesAreSupported#
Check whether the device supports accessing files.
Parameters:
- hMap Device Node map handle.
- pResult Returns true if files are supported.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Check whether the device supports accessing files.
function GenApiFileWrite#
Writes binary data to a file.
Parameters:
- hFile The file handle.
- pBuffer The data buffer.
- length Specifies the number of bytes to write.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Writes binary data to a file.
function GenApiFloatGetMax#
Get a node's maximum floating-point value.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the maximum floating-point value of a node.
function GenApiFloatGetMin#
Get a node's minimum floating-point value.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the minimum floating-point value of a node.
function GenApiFloatGetRepresentation#
Get a node's preferred representation.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the preferred representation for the node's value. This value is a hint telling how the value should best be represented in a graphical user interface.
function GenApiFloatGetUnit#
Return a floating-point node's unit.
Parameters:
- hNode Node to operate on
- pBuf Buffer to receive result
- pBufLen Result buffer size
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for the unit that applies to its value. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiFloatGetValue#
Get a node's floating-point value without validation.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the floating-point value of a node. No validation is performed on the value returned.
function GenApiFloatGetValueEx#
Return a node's floating-point value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the floating-point value of a node. If verify equals true, the result value is checked to ensure that it does not violate any of the node's constraints.
function GenApiFloatSetValue#
Set a node's floating-point value with mandatory validation.
Parameters:
- hNode Node to operate on
- value Value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular value. The function will fail if the value to be set conflicts with any relevant constraints.
function GenApiFloatSetValueEx#
Set a node's floating-point value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- value Value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular value. If verify equals true, the function will fail if the value to be set conflicts with any relevant constraints.
function GenApiGetLastErrorDetail#
Get detailed textual description for the latest error details, e.g. the origin of the error.
Parameters:
- pBuf Pointer to the user-supplied character buffer, or
NULL
- pBufLen Pointer to the actual buffer size
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Whenever a function reports an error, it also sets up a string that describes the error in more detail than the brief error message returned by GenApiGetLastErrorMessage(). This function can be used to retrieve that description by copying it to a user-provided buffer. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiGetLastErrorMessage#
Get a brief textual description of the latest error.
Parameters:
- pBuf Pointer to user-supplied character buffer, or
NULL
- pBufLen Pointer to the actual buffer size
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Whenever a function reports an error, it also sets up a string description for it. This function can be used to retrieve that description by copying it to a user-provided buffer. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiIntegerGetInc#
Get the value increment from an integer node.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the integer value increment of a node.
function GenApiIntegerGetIncInt32#
Get the value increment from an integer node.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the integer value increment of a node.
function GenApiIntegerGetMax#
Get the maximum value from an integer node.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the maximum integer value of a node.
function GenApiIntegerGetMaxInt32#
Get the maximum value from an integer node.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the maximum integer value of a node.
function GenApiIntegerGetMin#
Get the minimum value from an integer node.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the minimum integer value of a node.
function GenApiIntegerGetMinInt32#
Get the minimum value from an integer node.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the minimum integer value of a node.
function GenApiIntegerGetRepresentation#
Get a node's preferred representation.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the preferred representation for the node's value. This value is a hint telling how the value should best be represented in a graphical user interface.
function GenApiIntegerGetValue#
Get a node's integer value without validation.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the integer value of a node. No validation is performed on the value returned.
function GenApiIntegerGetValueEx#
Return a node's integer value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the integer value of a node. If verify equals true, the result value is checked to ensure that it does not violate any of the node's constraints.
function GenApiIntegerGetValueExInt32#
Return a node's integer value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the integer value of a node. If verify equals true, the result value is checked to ensure that it does not violate any of the node's constraints.
function GenApiIntegerGetValueInt32#
Get a node's integer value without validation.
Parameters:
- hNode Node to operate on
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the integer value of a node. No validation is performed on the value returned.
function GenApiIntegerSetValue#
Set a node's integer value with mandatory validation.
Parameters:
- hNode Node to operate on
- value Value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular value. The function will fail if the value to be set conflicts with any relevant constraints.
function GenApiIntegerSetValueEx#
Set a node's integer value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- value Value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular value. If verify equals true, the function will fail if the value to be set conflicts with any relevant constraints.
function GenApiIntegerSetValueExInt32#
Set a node's integer value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- value Value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular value. If verify equals true, the function will fail if the value to be set conflicts with any relevant constraints.
function GenApiIntegerSetValueInt32#
Set a node's integer value with mandatory validation.
Parameters:
- hNode Node to operate on
- value Value to set
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Set the node to a particular value. The function will fail if the value to be set conflicts with any relevant constraints.
function GenApiNodeDeregisterCallback#
Remove a node callback function.
Parameters:
- hNode Node to operate on
- hCb Callback handle
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Remove a callback function previously installed by GenApiNodeRegisterCallback() from a node.
function GenApiNodeFromString#
Set a node's value from a text string with mandatory validation.
Parameters:
- hNode Node to operate on
- pString Buffer containing text string
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
This function takes a text string in pString and tries to convert it to a value to set the node to. This may fail for a number of reasons, e.g. due to the node not being writeable or not having a value that could be set. The function will also fail if the value to be set conflicts with any relevant constraints.
function GenApiNodeFromStringEx#
Set a node's value from a text string with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- pString Buffer containing text string
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
This function takes a text string in pString and tries to convert it to a value to set the node to. This may fail for a number of reasons, e.g. due to the node not being writeable or not having a value that could be set. If verify equals true, the function will also fail if the value to be set conflicts with any relevant constraints.
function GenApiNodeGetAccessMode#
Query node for allowed access modes.
Parameters:
- hNode Node to operate on
- pAccessMode Pointer to variable receiving access mode
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
The value returned in the variable pointed to by pAccessMode indicates what kinds of access are allowed for the node referred to by hNode.
function GenApiNodeGetAlias#
Get a node's alias.
Parameters:
- hNode Node to operate on
- phNode Result pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
This function returns a node's alias if available. An invalid handle is returned if no alias exists. If an alias exists, a handle for the alias node is returned in the variable pointed to by phNode.
function GenApiNodeGetCachingMode#
Query node for its caching mode.
Parameters:
- hNode Node to operate on
- pCachingMode Pointer to variable receiving result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Caching may be implemented differently for nodes with different characteristics. There is an enumerated type EGenApiCachingMode that is used to encode the caching strategy for a particular node. Use this function to get a node's caching mode.
function GenApiNodeGetDescription#
Return a node's description text.
Parameters:
- hNode Node to operate on
- pBuf Buffer to receive result
- pBufLen Result buffer size on input and buffer size needed on output
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for its associated 'description' text. This is a text string describing the node and its purpose in some more detail than GenApiNodeGetToolTip(), suitable for being displayed as an on-line help by interactive programs that offer access to the node. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiNodeGetDisplayName#
Return a node's user-friendly name.
Parameters:
- hNode Node to operate on
- pBuf Buffer to receive result
- pBufLen Result buffer size on input and buffer size needed on output
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for its associated 'user-friendly' name. While the node name returned by GenApiNodeGetName() is meant to be a unique identification tag, this is a more descriptive name meant to be used to identify a node in a dialog. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiNodeGetName#
Return a node's name.
Parameters:
- hNode Node to operate on
- pBuf Buffer to receive result
- pBufLen Result buffer size on input and buffer size needed on output
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for its name. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiNodeGetNameSpace#
Return a node's name space.
Parameters:
- hNode Node to operate on
- pNamespace Pointer to variable receiving name space
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for the name space (custom or standard) it belongs to.
function GenApiNodeGetPollingTime#
Query a node for its recommended polling interval.
Parameters:
- hNode Node to operate on
- pPollingTime Pointer to variable receiving result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Nodes that are subject to asynchronous state changes must be periodically queried (polled) in order to detect state changes. Such nodes have an associated attribute specifying a recommended polling interval in milliseconds. Use this function to get that value.
function GenApiNodeGetPollingTimeInt32#
Query a node for its recommended polling interval.
Parameters:
- hNode Node to operate on
- pPollingTime Pointer to variable receiving result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Nodes that are subject to asynchronous state changes must be periodically queried (polled) in order to detect state changes. Such nodes have an associated attribute specifying a recommended polling interval in milliseconds. Use this function to get that value.
function GenApiNodeGetToolTip#
Return a node's tool tip text.
Parameters:
- hNode Node to operate on
- pBuf Buffer to receive result
- pBufLen Result buffer size on input and buffer size needed on output
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for its associated 'tool tip' text. This is a text string briefly describing the node and its purpose, suitable for being displayed as a pop-up by interactive programs that offer access to the node. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiNodeGetType#
Get node type.
Parameters:
- hNode Node to operate on
- pType Result pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for its type.
function GenApiNodeGetVisibility#
Return a node's visibility.
Parameters:
- hNode Node to operate on
- pVisibility Pointer to variable receiving visibility
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Query the node represented by hNode for its level of visibility (Beginner, Expert, Guru, or Invisible).
function GenApiNodeImposeAccessMode#
Modify a node's accessibility.
Parameters:
- hNode Node to operate on
- imposedAccessMode Desired new access mode
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Whether a particular node allows read, write, or any access at all, is encoded in its access mode. The original access mode for a node, which is computed taking into account node interdependencies, can be further restricted by means of this function. It is not possible to set the access mode to one more permissive than the original mode. An attempt to do so will be ignored.
function GenApiNodeImposeVisibility#
Modify a node's visibility.
Parameters:
- hNode Node to operate on
- imposedVisibility Desired new visibility
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
A particular node is only visible if the current user level is set at least as high as the node's visibility. This function can be used to further limit a node's visibility. The function cannot be used to increase a node's visibility (so that it would become visible at a lower user level). Any attempt to do so will have no effect.
function GenApiNodeInvalidateNode#
Mark node as possibly changed.
Parameters:
- hNode Node to operate on
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Calling this function invalidates the currently cached status for the node. Then, callbacks for all dependent nodes are triggered.
function GenApiNodeIsAvailable#
Check whether a feature's value is available.
Parameters:
- hNode Node to operate on
- pResult Pointer to variable receiving boolean result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Check whether the value of the feature represented by hNode is currently accessible (GenApiNodeGetAccessMode() returns neither NA nor NI).
function GenApiNodeIsImplemented#
Check whether a feature is implemented.
Parameters:
- hNode Node to operate on
- pResult Pointer to variable receiving boolean result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Check whether the feature represented by hNode is actually implemented (GenApiNodeGetAccessMode() returns not NI).
function GenApiNodeIsReadable#
Check whether a feature's value is readable.
Parameters:
- hNode Node to operate on
- pResult Pointer to variable receiving boolean result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Check whether the value of the feature represented by hNode can be read (GenApiNodeGetAccessMode() returns RO or RW).
function GenApiNodeIsWritable#
Check whether a feature's value is writable.
Parameters:
- hNode Node to operate on
- pResult Pointer to variable receiving boolean result
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Check whether the value of the feature represented by hNode can be written (GenApiNodeGetAccessMode() returns WO or RW).
function GenApiNodeMapGetNode#
GENAPIC_RESULT GenApiNodeMapGetNode(
NODEMAP_HANDLE hMap,
const char * pName,
NODE_HANDLE * phNode
)
Find a node by its name.
Parameters:
- hMap Node map handle
- pName Node name to find
- phNode Result pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Use this function to search a node map for a node with a given name. An invalid handle is returned if not found. If found, a handle for the node is returned in the variable pointed to by phNode.
function GenApiNodeMapGetNodeByIndex#
GENAPIC_RESULT GenApiNodeMapGetNodeByIndex(
NODEMAP_HANDLE hMap,
size_t index,
NODE_HANDLE * phNode
)
Find a node by its index.
Parameters:
- hMap Node map handle
- index Index of node to get
- phNode Result pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Translate a numerical index to a node handle. By using GenApiNodeMapGetNumNodes() to get the number of nodes in a node map, this function can be used to get a handle for every node contained, without having to know its name.
function GenApiNodeMapGetNumNodes#
Get the number of nodes contained in a node map.
Parameters:
- hMap Node map handle
- pValue Result value pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Return the number of nodes contained in a node map. This value can be used to traverse a node map, visiting every node using GenApiNodeMapGetNodeByIndex().
function GenApiNodeMapPoll#
Poll all nodes in a node map.
Parameters:
- hMap Node map handle
- timestamp Current time stamp in ms
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Poll all nodes in the node map and execute callbacks for those that are expired.
function GenApiNodeMapPollInt32#
Poll all nodes in a node map.
Parameters:
- hMap Node map handle
- timestamp Current time stamp in ms
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Poll all nodes in the node map and execute callbacks for those that are expired.
function GenApiNodeRegisterCallback#
GENAPIC_RESULT GenApiNodeRegisterCallback(
NODE_HANDLE hNode,
NodeCallbackFunction_t * pCbFunction,
NODE_CALLBACK_HANDLE * phCb
)
Install a node callback function.
Parameters:
- hNode Node to operate on
- pCbFunction Callback function pointer
- phCb Callback handle
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Note If you need to perform special processing whenever the node's value changes you need to retrieve the value using any of the GetValue functions.
Install a callback function, to be called whenever any of the node's attributes changes. This also includes the access mode of the node.
The callback handle returned can be used to remove the callback using GenApiNodeDeregisterCallback().
function GenApiNodeToString#
Return a textual representation of a node's value.
Parameters:
- hNode Node to operate on
- pBuf Buffer to receive result
- pBufLen Result buffer size
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Convert a node's value to a human-readable text string. The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiNodeToStringEx#
GENAPIC_RESULT GenApiNodeToStringEx(
NODE_HANDLE hNode,
_Bool verify,
char * pBuf,
size_t * pBufLen
)
Return a textual representation of a node's value with optional validation.
Parameters:
- hNode Node to operate on
- verify Boolean switch to enable validation
- pBuf Buffer to receive result
- pBufLen Result buffer size
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Convert a node's value to a human-readable text string, with optional validation. If verify equals true, the node's value is first checked against any relevant constraints, and an error is returned if the value is invalid. This check is not done if verify equals false, in this case, the function behaves identically to GenApiNodeToString(). The buffer passed to this function must be large enough to hold the entire string, including a terminating zero. If the function is called with pBuf set to NULL
, the variable pointed to by pBufLen is set to the required buffer size.
function GenApiPortRead#
Perform a raw read on the port implemented by the node passed.
Parameters:
- hNode Node of the port to read from. Use GenApiNodeMapGetNode to get the node handle.
- pBuffer Points to the buffer to copy the data to.
- Address Address to start reading data from.
- Length Number of bytes to read starting at Address.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Reads raw data from a port implemented by a node. Some nodes (i.e. the "Device" node) can be used to read- and write directly to the device. Specify the address from where to read data. The count of data bytes passed in Length
is read. The data read will be written to the buffer passed in pBuffer. Make sure the buffer has at least a size of Length-bytes.
function GenApiPortWrite#
GENAPIC_RESULT GenApiPortWrite(
NODE_HANDLE hNode,
const void * pBuffer,
int64_t Address,
size_t Length
)
Perform a raw write on the port implemented by the node passed.
Parameters:
- hNode Node of the port to write to. Use GenApiNodeMapGetNode to get the node handle.
- pBuffer Points to the buffer to read the data.
- Address Address where to start writing data to.
- Length Number of bytes to write starting at Address.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Writes raw data to a port implemented by a node. Some nodes (i.e. the "Device" node) can be used to read- and write directly to the device. Specify the address from where to read data. The count of data bytes passed in Length
is read. The data written will be read from the buffer passed in pBuffer. Make sure the buffer has at least a size of Length-bytes.
function GenApiRegisterGetAddress#
Returns the address of the register node.
Parameters:
- hNode Node to operate on. Use GenApiNodeMapGetNode() to get the node handle.
- pAddress On sucessful return, the value points to the register address of the node. This parameter must not be NULL.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Returns the length in bytes of the register node. You can use the returned value when calling GenApiRegisterGetValue() or GenApiRegisterSetValue().
function GenApiRegisterGetLength#
Returns the length in bytes of the register node.
Parameters:
- hNode Node to operate on. Use GenApiNodeMapGetNode() to get the node handle.
- pLength On successful return, the value points to the length in bytes of the register node. This parameter must not be NULL.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Returns the length in bytes of the register node. You can use the returned value when calling GenApiRegisterGetValue() or GenApiRegisterSetValue().
function GenApiRegisterGetValue#
Reads binary data from the register node.
Parameters:
- hNode Node to operate on. Use GenApiNodeMapGetNode() to get the node handle.
- pBuffer Points to the buffer for storing the data read from the node. This parameter must not be NULL.
- pLength On input, the value points to size in bytes of the buffer passed in pBuffer. Use GenApiRegisterGetLength() to get the length of the register. On successful return, it will point to the number of bytes written to pBuffer. This parameter must not be NULL.
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Read binary data from a register node. The data retrieved will be written to the buffer passed in pBuffer. You can retrieve the length of the register by calling GenApiRegisterGetLength().
function GenApiRegisterSetValue#
Writes binary data to the register node.
Parameters:
- hNode Node to operate on. Use GenApiNodeMapGetNode() to get the node handle.
- pBuffer Points to the buffer holding the data to write to the node. This parameter must not be NULL.
- length The number of bytes of the buffer passed in pBuffer. Use GenApiRegisterGetLength() to get the length of the register. This parameter must be less or equal to the value returned by GenApiRegisterGetLength().
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Writes binary data to a register node. You can retrieve the length of the register by calling GenApiRegisterGetLength().
function GenApiSelectorGetNumSelectedFeatures#
Return the number of selected nodes.
Parameters:
- hNode Node to operate on
- pValue Number of selected nodes
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Returns the number of nodes selected by this node.
function GenApiSelectorGetNumSelectingFeatures#
Return the number of selecting features.
Parameters:
- hNode Node to operate on
- pValue Number of selecting features
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
Returns the number of features selecting this node.
function GenApiSelectorGetSelectedFeatureByIndex#
GENAPIC_RESULT GenApiSelectorGetSelectedFeatureByIndex(
NODE_HANDLE hNode,
size_t index,
NODE_HANDLE * phNode
)
Get a selected node by its index.
Parameters:
- hNode Node to operate on
- index Index in selected nodes
- phNode result node handle pointer of the selected node
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
A feature node may select one or more other features. This function returns a NODE_HANDLE for a selected node identified by its index. Using the value returned by GenApiNodeGetNumSelectedFeatures(), this can be used to implement a loop to iterate over all selected nodes of a given node.
function GenApiSelectorGetSelectingFeatureByIndex#
GENAPIC_RESULT GenApiSelectorGetSelectingFeatureByIndex(
NODE_HANDLE hNode,
size_t index,
NODE_HANDLE * phNode
)
Return a selecting feature by its index.
Parameters:
- hNode Node to operate on
- index Index in selectors
- phNode result node handle pointer
Return: If the function succeeds, the return value is GENAPI_E_OK.
If the function fails, the return value will be any of error codes described in the section ErrorCodes.
A feature node may be selected by one or more other features. This function returns a NODE_HANDLE for a selector node identified by its index. Using the value returned by GenApiNodeGetNumSelectingFeatures(), this can be used to implement a loop to iterate over all selectors of a given node.
Macros Documentation#
define GENAPIC_INVALID_HANDLE#
A value for invalid / uninitialized handles.