Instant Camera#
モジュール#
名前 |
---|
Universal Instant Camera for All Basler Devices The Universal Instant Camera for All Basler Devices extends the Instant Camera. |
クラス#
名前 | |
---|---|
class | Pylon::CAcquireContinuousConfiguration Changes the configuration of the camera to free-running continuous acquisition. |
class | Pylon::CAcquireSingleFrameConfiguration An instant camera configuration for single frame acquisition, Use together with CInstantCamera::GrabOne() only. |
class | Pylon::CCameraEventHandler The camera event handler base class. |
class | Pylon::CConfigurationEventHandler The configuration event handler base class. |
class | Pylon::CConfigurationHelper Helper functions for different camera configuration classes. |
class | Pylon::CGrabResultData Makes the data for one grabbed buffer available. |
class | Pylon::CGrabResultPtr A smart pointer holding a reference to grab result data. |
class | Pylon::CImageEventHandler The image event handler base class. |
class | Pylon::CInstantCamera Provides convenient access to a camera device. |
class | Pylon::CInstantCameraArray Supports grabbing with multiple camera devices. |
class | Pylon::CSoftwareTriggerConfiguration Changes the configuration of the camera so that the acquisition of frames is triggered by software trigger. |
class | Pylon::IBufferFactory Usable to create a custom buffer factory when needed. |
タイプ#
名前 | |
---|---|
enum | ECleanup { Cleanup_None, Cleanup_Delete} Defines who deletes a passed object if it is not needed anymore. |
enum | ERegistrationMode { RegistrationMode_Append, RegistrationMode_ReplaceAll} Defines how to register an item. |
enum | ETimeoutHandling { TimeoutHandling_Return, TimeoutHandling_ThrowException} Defines how to handle a timeout for a method. |
enum | EGrabStrategy { GrabStrategy_OneByOne, GrabStrategy_LatestImageOnly, GrabStrategy_LatestImages, GrabStrategy_UpcomingImage} Lists the possible grab strategies. |
enum | EGrabLoop { GrabLoop_ProvidedByInstantCamera, GrabLoop_ProvidedByUser} Defines the use of an additional grab loop thread. |
enum | ECameraEventAvailability { CameraEventAvailability_Mandatory, CameraEventAvailability_Optional} Defines how to register a camera event handler. |
enum | EPayloadType { PayloadType_Undefined = -1, PayloadType_Image, PayloadType_RawData, PayloadType_File, PayloadType_ChunkData, PayloadType_GenDC, PayloadType_DeviceSpecific = 0x8000} Possible payload type values. |
Functions#
名前 | |
---|---|
const VersionInfo | Sfnc_VersionUndefined(0 , 0 , 0 ) Constant for undefined SFNC version. |
const VersionInfo | Sfnc_1_2_1(1 , 2 , 1 ) Constant for SFNC version 1.2.1. |
const VersionInfo | Sfnc_1_3_0(1 , 3 , 0 ) Constant for SFNC version 1.3.0. |
const VersionInfo | Sfnc_1_4_0(1 , 4 , 0 ) Constant for SFNC version 1.4.0. |
const VersionInfo | Sfnc_1_5_0(1 , 5 , 0 ) Constant for SFNC version 1.5.0. |
const VersionInfo | Sfnc_1_5_1(1 , 5 , 1 ) Constant for SFNC version 1.5.1. |
const VersionInfo | Sfnc_2_0_0(2 , 0 , 0 ) Constant for SFNC version 2.0.0. This version or a later version is used by USB camera devices. |
const VersionInfo | Sfnc_2_1_0(2 , 1 , 0 ) Constant for SFNC version 2.1.0. |
const VersionInfo | Sfnc_2_2_0(2 , 2 , 0 ) Constant for SFNC version 2.2.0. |
const VersionInfo | Sfnc_2_3_0(2 , 3 , 0 ) Constant for SFNC version 2.3.0. |
const VersionInfo | Sfnc_2_4_0(2 , 4 , 0 ) Constant for SFNC version 2.4.0. |
const VersionInfo | Sfnc_2_5_0(2 , 5 , 0 ) Constant for SFNC version 2.5.0. |
Detailed Description#
Instant Camera classes make it possible to grab images with a few lines of code reducing the programming effort to a minimum.
You can find more information here:
Types Documentation#
enum ECleanup#
Enumerator | 値 | 説明 |
---|---|---|
Cleanup_None | The caller is responsible for deleting the passed object. The object needs to be detached or deregistered before deletion. | |
Cleanup_Delete | The passed object is deleted if it is not needed anymore. |
Defines who deletes a passed object if it is not needed anymore.
enum ERegistrationMode#
Enumerator | 値 | 説明 |
---|---|---|
RegistrationMode_Append | The item is appended to the list of registered items. | |
RegistrationMode_ReplaceAll | The item replaces all other registered items. |
Defines how to register an item.
enum ETimeoutHandling#
Enumerator | 値 | 説明 |
---|---|---|
TimeoutHandling_Return | The method returns on timeout. What data is returned can be found in the documentation of the method. | |
TimeoutHandling_ThrowException | An exception is thrown on timeout. |
Defines how to handle a timeout for a method.
enum EGrabStrategy#
Enumerator | 値 | 説明 |
---|---|---|
GrabStrategy_OneByOne | The images are processed in the order of their arrival. This is the default grab strategy. | |
GrabStrategy_LatestImageOnly | Only the latest image is kept in the output queue, all other grabbed images are skipped. If no image is in the output queue when retrieving an image with CInstantCamera::RetrieveResult(), the processing waits for the upcoming image. | |
GrabStrategy_LatestImages | This strategy can be used to grab images while keeping only the latest images. If the application does not retrieve all images in time, all other grabbed images are skipped. The CInstantCamera::OutputQueueSize parameter can be used to control how many images can be queued in the output queue. When setting the output queue size to 1, this strategy is equivalent to GrabStrategy_LatestImageOnly grab strategy. When setting the output queue size to CInstantCamera::MaxNumBuffer, this strategy is equivalent to GrabStrategy_OneByOne. | |
GrabStrategy_UpcomingImage | The input buffer queue is kept empty. This prevents grabbing. However, when retrieving an image with a call to the CInstantCamera::RetrieveResult() method a buffer is queued into the input queue and then the call waits for the upcoming image. The buffer is removed from the queue on timeout. Hence after the call to the CInstantCamera::RetrieveResult() method the input buffer queue is empty again. The upcoming image grab strategy cannot be used together with USB or GenTL-based camera devices. See the advanced topics section of the pylon Programmer's Guide for more information. |
Lists the possible grab strategies.
enum EGrabLoop#
Enumerator | 値 | 説明 |
---|---|---|
GrabLoop_ProvidedByInstantCamera | The grab loop thread is provided by the Instant Camera. It calls RetrieveResult() in a loop. Grabbed images are processed by registered image event handlers. The grab loop thread is started when the grab starts. | |
GrabLoop_ProvidedByUser | The user code calls RetrieveResult() in a loop to process grabbed images and camera events. |
Defines the use of an additional grab loop thread.
enum ECameraEventAvailability#
Enumerator | 値 | 説明 |
---|---|---|
CameraEventAvailability_Mandatory | The camera event must be provided by the camera, otherwise an exception is thrown. | |
CameraEventAvailability_Optional | The camera event handler is not used if the camera does not support the camera event. |
Defines how to register a camera event handler.
enum EPayloadType#
Enumerator | 値 | 説明 |
---|---|---|
PayloadType_Undefined | -1 | Undefined payload. |
PayloadType_Image | The buffer contains image data. | |
PayloadType_RawData | The buffer contains raw data. | |
PayloadType_File | The buffer contains file data. | |
PayloadType_ChunkData | The buffer contains chunk data. | |
PayloadType_GenDC | The buffer contains GenDC container. | |
PayloadType_DeviceSpecific | 0x8000 | The buffer contains device specific data. |
Possible payload type values.
Functions Documentation#
function Sfnc_VersionUndefined#
Constant for undefined SFNC version.
function Sfnc_1_2_1#
Constant for SFNC version 1.2.1.
function Sfnc_1_3_0#
Constant for SFNC version 1.3.0.
function Sfnc_1_4_0#
Constant for SFNC version 1.4.0.
function Sfnc_1_5_0#
Constant for SFNC version 1.5.0.
function Sfnc_1_5_1#
Constant for SFNC version 1.5.1.
function Sfnc_2_0_0#
Constant for SFNC version 2.0.0. This version or a later version is used by USB camera devices.
function Sfnc_2_1_0#
Constant for SFNC version 2.1.0.
function Sfnc_2_2_0#
Constant for SFNC version 2.2.0.
function Sfnc_2_3_0#
Constant for SFNC version 2.3.0.
function Sfnc_2_4_0#
Constant for SFNC version 2.4.0.
function Sfnc_2_5_0#
Constant for SFNC version 2.5.0.