PLCamera.BinningModeVerticalEnum Class#
Applies to: CameraLink
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BinningModeVerticalEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BinningModeVerticalEnum | Initializes a new instance of the PLCamera.BinningModeVerticalEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Averaging | The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light. Applies to: CameraLink | |
名前 | The full name of BinningModeVertical (Overrides ParameterListEnum.Name.) | |
Summing | The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio. Applies to: CameraLink |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BinningModeVertical (Overrides Object.ToString()()()().) |
PLCamera.BinningModeVerticalEnum.ToString Method#
The full name of BinningModeVertical
Return Value#
Type: String
Returns the full name of BinningModeVertical
PLCamera.BinningModeVerticalEnum Constructor#
Initializes a new instance of the PLCamera.BinningModeVerticalEnum class
PLCamera.BinningModeVerticalEnum.Averaging Property#
The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light.
Applies to: CameraLink
PLCamera.BinningModeVerticalEnum.Name Property#
The full name of BinningModeVertical
PLCamera.BinningModeVerticalEnum.Summing Property#
The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio.
Applies to: CameraLink