すべてのBaslerデバイスに対応するユニバーサルインスタントカメラ#
The Universal Instant Camera for All Basler Devices extends the Instant Camera. More…
クラス#
名前 | |
---|---|
class | Pylon::CBaslerUniversalCameraEventHandler The camera event handler base class. |
class | Pylon::CBaslerUniversalConfigurationEventHandler The configuration event handler base class. |
class | Pylon::CBaslerUniversalGrabResultData The Universal grab result data. |
class | Pylon::CBaslerUniversalGrabResultPtr The Universal grab result smart pointer. |
class | Pylon::CBaslerUniversalImageEventHandler The image event handler base class. |
struct | Pylon::CBaslerUniversalInstantCameraTraits Lists all the types used by the universal instant camera class. |
class | Pylon::CBaslerUniversalInstantCamera Extends the CInstantCamera by universal parameter interface classes combining all interface types. |
class | Pylon::CBaslerUniversalInstantCameraArray Universal instant camera array. |
class | Pylon::CActionTriggerConfiguration Changes the configuration of the camera so that it is triggered by the first available action command. |
Detailed Description#
The Universal Instant Camera for All Basler Devices extends the Instant Camera.
This means that all features of the base class Pylon::CInstantCamera are also available. You can find more information here: