PLCamera.TimerSequenceTimerSelectorEnum Class#
Visibility: Guru
Selected by: TimerSequenceEntrySelector
Selecting Parameters: TimerSequenceTimerDelayRaw, TimerSequenceTimerDurationRaw, TimerSequenceTimerEnable, TimerSequenceTimerInverter
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TimerSequenceTimerSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.TimerSequenceTimerSelectorEnum | Initializes a new instance of the PLCamera.TimerSequenceTimerSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of TimerSequenceTimerSelector (Overrides ParameterListEnum.Name.) | |
Timer1 | ||
Timer2 | ||
Timer3 | ||
Timer4 |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TimerSequenceTimerSelector (Overrides Object.ToString()()()().) |
PLCamera.TimerSequenceTimerSelectorEnum.ToString Method#
The full name of TimerSequenceTimerSelector
Return Value#
Type: String
Returns the full name of TimerSequenceTimerSelector
PLCamera.TimerSequenceTimerSelectorEnum Constructor#
Initializes a new instance of the PLCamera.TimerSequenceTimerSelectorEnum class
PLCamera.TimerSequenceTimerSelectorEnum.Name Property#
The full name of TimerSequenceTimerSelector