PLCamera.BslLightDeviceStrobeModeEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
Selected by: BslLightDeviceSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightDeviceStrobeModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslLightDeviceStrobeModeEnum | Initializes a new instance of the PLCamera.BslLightDeviceStrobeModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
自動 | The timing of the individual strobe pulses is determined by the Exposure Active signal. The light pulse will last for the duration of the exposure, up to a maximum of 655 350 microseconds. Applies to: GigE and ace USB | |
手動 | The timing of the individual strobe pulses can be specified manually using the Light Device Strobe Duration parameter. Applies to: GigE and ace USB | |
名前 | The full name of BslLightDeviceStrobeMode (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslLightDeviceStrobeMode (Overrides Object.ToString()()()().) |
PLCamera.BslLightDeviceStrobeModeEnum.ToString Method#
The full name of BslLightDeviceStrobeMode
Return Value#
Type: String
Returns the full name of BslLightDeviceStrobeMode
PLCamera.BslLightDeviceStrobeModeEnum Constructor#
Initializes a new instance of the PLCamera.BslLightDeviceStrobeModeEnum class
PLCamera.BslLightDeviceStrobeModeEnum.Automatic Property#
The timing of the individual strobe pulses is determined by the Exposure Active signal. The light pulse will last for the duration of the exposure, up to a maximum of 655 350 microseconds.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceStrobeModeEnum.Manual Property#
The timing of the individual strobe pulses can be specified manually using the Light Device Strobe Duration parameter.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceStrobeModeEnum.Name Property#
The full name of BslLightDeviceStrobeMode