PLPixelDataConverter.InconvertibleEdgeHandlingEnum Class#
Visibility: Beginner
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLPixelDataConverter.InconvertibleEdgeHandlingEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLPixelDataConverter.InconvertibleEdgeHandlingEnum | Initializes a new instance of the PLPixelDataConverter.InconvertibleEdgeHandlingEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Clip | Rows and columns that can't be converted are removed from the output image. | |
Extend | Rows and columns that can't be converted are filled by extrapolating image data from neighboring rows and columns. | |
名前 | The full name of InconvertibleEdgeHandling (Overrides ParameterListEnum.Name.) | |
SetZero | Rows and columns that can't be converted are set to zero. |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of InconvertibleEdgeHandling (Overrides Object.ToString()()()().) |
PLPixelDataConverter.InconvertibleEdgeHandlingEnum.ToString Method#
The full name of InconvertibleEdgeHandling
Return Value#
Type: String
Returns the full name of InconvertibleEdgeHandling
PLPixelDataConverter.InconvertibleEdgeHandlingEnum Constructor#
Initializes a new instance of the PLPixelDataConverter.InconvertibleEdgeHandlingEnum class
PLPixelDataConverter.InconvertibleEdgeHandlingEnum.Clip Property#
Rows and columns that can't be converted are removed from the output image.
PLPixelDataConverter.InconvertibleEdgeHandlingEnum.Extend Property#
Rows and columns that can't be converted are filled by extrapolating image data from neighboring rows and columns.
PLPixelDataConverter.InconvertibleEdgeHandlingEnum.Name Property#
The full name of InconvertibleEdgeHandling
PLPixelDataConverter.InconvertibleEdgeHandlingEnum.SetZero Property#
Rows and columns that can't be converted are set to zero.