IpConfigurator Class#
Inheritance Hierarchy#
System.Object
Basler.Pylon.IpConfigurator
Syntax#
C#
VB
The IpConfigurator type exposes the following members.
方法#
名前 | 説明 | |
---|---|---|
AnnounceRemoteDevice | Announce that a remote device is going to be used. | |
ChangeIpConfiguration(String, IpConfigurationMethod) | Change the IP configuration of a camera device. | |
ChangeIpConfiguration(String, IpConfigurationMethod, String, String, String) | Change the IP configuration of a camera device. | |
EnumerateAllDevices | Enumerates all available GigE Vision devices. | |
IsAutoIpActive | Checks if camera device is working in automatic IP configuration, also known as link-local address. | |
IsAutoIpSupported | Checks if camera device supports automatic IP configuration, also known as link-local address. | |
IsDhcpActive | Checks if camera device is working in DHCP configuration. | |
IsDhcpSupported | Checks if camera device supports DHCP configuration. | |
IsPersistentIpActive | Checks if camera device is working in persistent IP configuration, also known as static IP configuration. | |
IsPersistentIpSupported | Checks if camera device supports persistent IP configuration, also known as static IP configuration. | |
RenounceRemoteDevice | Stop using remote device. |
IpConfigurator.AnnounceRemoteDevice Method#
Announce that a remote device is going to be used.
Syntax#
C#
VB
パラメーター#
- ipAddress
- Type: System.String
Address of device in "dot notation".
Return Value#
Type: ICameraInfo
Returns ICameraInfo if the camera device is found.
Remarks#
This is necessary when working with IP-based camera devices that are behind a router.In order to succeed, that camera device must be reachable and a route configured.Most system setups will not need this.If all your camera devices are found using the CameraFinder, you will not need this.The announcement can be reverted using RenounceRemoteDevice().
Please note that devices announced using this function are only remembered temporarily. If you annouce a device and then stop using pylon in your program, the underlying pylon might get disposed and the information about announced devices is lost. It is recommended to hold at least one pylon object from the time this function is called to the time the device is opened.
IpConfigurator.ChangeIpConfiguration Method (String, IpConfigurationMethod)#
Change the IP configuration of a camera device.
Syntax#
C#
VB
Public Shared Function ChangeIpConfiguration (
macAddress As String,
method As IpConfigurationMethod
) As Boolean
パラメーター#
- macAddress
- Type: System.String
The MAC address of the camera device. - 決定して
- Type: Basler.Pylon.IpConfigurationMethod
The IpConfigurationMethod to be used.
Return Value#
Type: Boolean
Returns true if successful, false otherwise.
Remarks#
This overloaded method is for AutoIP or DHCP. To configure a static IP address, use the other overload.
IpConfigurator.ChangeIpConfiguration Method (String, IpConfigurationMethod, String, String, String)#
Change the IP configuration of a camera device.
Syntax#
C#
public static bool ChangeIpConfiguration(
string macAddress,
IpConfigurationMethod method,
string ipAddress,
string subnetMask,
string defaultGateway
)
VB
Public Shared Function ChangeIpConfiguration (
macAddress As String,
method As IpConfigurationMethod,
ipAddress As String,
subnetMask As String,
defaultGateway As String
) As Boolean
パラメーター#
- macAddress
- Type: System.String
The MAC address of the camera device. - 決定して
- Type: Basler.Pylon.IpConfigurationMethod
The IpConfigurationMethod to be used. - ipAddress
- Type: System.String
The target IP address of the camera device. - subnetMask
- Type: System.String
The target subnet mask of the camera device. - defaultGateway
- Type: System.String
The target default gateway of the camera device.
Return Value#
Type: Boolean
Returns true if successful, false otherwise.
Remarks#
This overloaded method is for a static IP address. To configure AutoIP or DHCP, use the other overload.
IpConfigurator.EnumerateAllDevices Method#
Enumerates all available GigE Vision devices.
Syntax#
C#
VB
Return Value#
Type: List(ICameraInfo)
Returns a list of ICameraInfo objects, one per camera found.
IpConfigurator.IsAutoIpActive Method#
Checks if camera device is working in automatic IP configuration, also known as link-local address.
Syntax#
C#
VB
パラメーター#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device.
Return Value#
Type: Boolean
Returns true if active, false otherwise.
IpConfigurator.IsAutoIpSupported Method#
Checks if camera device supports automatic IP configuration, also known as link-local address.
Syntax#
C#
VB
パラメーター#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device.
Return Value#
Type: Boolean
Returns true if supported, false otherwise.
IpConfigurator.IsDhcpActive Method#
Checks if camera device is working in DHCP configuration.
Syntax#
C#
VB
パラメーター#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device.
Return Value#
Type: Boolean
Returns true if active, false otherwise.
IpConfigurator.IsDhcpSupported Method#
Checks if camera device supports DHCP configuration.
Syntax#
C#
VB
パラメーター#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device.
Return Value#
Type: Boolean
Returns true if supported, false otherwise.
IpConfigurator.IsPersistentIpActive Method#
Checks if camera device is working in persistent IP configuration, also known as static IP configuration.
Syntax#
C#
VB
パラメーター#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device.
Return Value#
Type: Boolean
Returns true if active, false otherwise.
IpConfigurator.IsPersistentIpSupported Method#
Checks if camera device supports persistent IP configuration, also known as static IP configuration.
Syntax#
C#
VB
パラメーター#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device.
Return Value#
Type: Boolean
Returns true if supported, false otherwise.
IpConfigurator.RenounceRemoteDevice Method#
Stop using remote device.
Syntax#
C#
VB
パラメーター#
- ipAddress
- Type: System.String
Address of device in "dot notation".
Return Value#
Type: Boolean
Returns true if successful, false otherwise.
IpConfigurator.ChangeIpConfiguration Method#
Overload List#
名前 | 説明 | |
---|---|---|
ChangeIpConfiguration(String, IpConfigurationMethod) | Change the IP configuration of a camera device. | |
ChangeIpConfiguration(String, IpConfigurationMethod, String, String, String) | Change the IP configuration of a camera device. |