Library Class#
Inheritance Hierarchy#
System.Object
Basler.Pylon.Library
Syntax#
C#
VB
The Library type exposes the following members.
Constructors#
名前 | 説明 | |
---|---|---|
ライブラリー | A Library object can be created to make sure that internal resources used by the Pylon library are not freed. This is only needed when AllowAutoRelease is set to true or if multiple assemblies use the pylonNET library. |
プロパティ#
名前 | 説明 | |
---|---|---|
VersionInfo | The current version of the library. |
方法#
名前 | 説明 | |
---|---|---|
Dispose | Releases a reference to the library. | |
EnumerateTransportLayers | Searches for information about available transport layers. | |
SetProperty | Sets a property in pylon. |
Remarks#
The library is initialized implicitly by using an object of the library, e.g. by creating a Camera
object, or by calling one of its static methods, e.g. CameraFinder.Enumerate()
. The internal resources of the library are freed when the application domain is unloaded.
Library.Dispose Method#
Releases a reference to the library.
Syntax#
C#
VB
Implements#
IDisposable.Dispose()
Remarks#
Thread Safety: This method is thread-safe.
Error Safety: Does not throw exceptions.
Library.EnumerateTransportLayers Method#
Searches for information about available transport layers.
Syntax#
C#
VB
Return Value#
Type: List(ITransportLayerInfo)
Returns a list transport layer info objects, one per transport layer.
Remarks#
The term 'transport layer' is used as an abstraction for a physical interface such as GigE or USB 3.0. For each of these interfaces, there are drivers providing access to camera devices. Thread Safety: This method is thread-safe.
Error Safety: Does not throw exceptions.
Library.SetProperty Method#
Sets a property in pylon.
Syntax#
C#
VB
パラメーター#
- propertyId
- Type: System.Int32
Identifier of the property. - data
- Type: System.Byte[]
Array with the value of the property.
Remarks#
Call this function to set the value of a property. Thread Safety: This method is thread-safe.
Error Safety: Can throw exceptions if the property could not be set.
Library Constructor#
A Library object can be created to make sure that internal resources used by the Pylon library are not freed. This is only needed when AllowAutoRelease is set to true or if multiple assemblies use the pylonNET library.
Syntax#
C#
VB
Remarks#
Thread Safety: This method is thread-safe.
Error Safety: Does not throw exceptions.
Library.VersionInfo Property#
The current version of the library.
Syntax#
C#
VB
Return Value#
Type: Version
Returns the current version of the Pylon library.
Remarks#
Thread Safety: This property is thread-safe.
Error Safety: Does not throw exceptions.