PLCamera.CxpConnectionTestModeEnum Class#
Applies to: boost CoaXPress and boost_V_CoaXPress
Visibility: Expert
Selected by: CxpConnectionSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpConnectionTestModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.CxpConnectionTestModeEnum | Initializes a new instance of the PLCamera.CxpConnectionTestModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Mode1 | Test mode is enabled. Applies to: boost CoaXPress and boost_V_CoaXPress | |
名前 | The full name of CxpConnectionTestMode (Overrides ParameterListEnum.Name.) | |
Off | Test mode is disabled. Applies to: boost CoaXPress and boost_V_CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of CxpConnectionTestMode (Overrides Object.ToString()()()().) |
PLCamera.CxpConnectionTestModeEnum.ToString Method#
The full name of CxpConnectionTestMode
Return Value#
Type: String
Returns the full name of CxpConnectionTestMode
PLCamera.CxpConnectionTestModeEnum Constructor#
Initializes a new instance of the PLCamera.CxpConnectionTestModeEnum class
PLCamera.CxpConnectionTestModeEnum.Mode1 Property#
Test mode is enabled.
Applies to: boost CoaXPress and boost_V_CoaXPress
PLCamera.CxpConnectionTestModeEnum.Name Property#
The full name of CxpConnectionTestMode
PLCamera.CxpConnectionTestModeEnum.Off Property#
Test mode is disabled.
Applies to: boost CoaXPress and boost_V_CoaXPress