Basler _UniversalInterfaceParams#
クラス#
名前 | |
---|---|
class | Basler_UniversalInterfaceParams::CUniversalInterfaceParams_Params A parameter class containing all parameters as members that are available for pylon interfaces. |
class | Basler_UniversalInterfaceParams::CUniversalInterfaceParams_Params_v7_4_0 A parameter class containing all parameters as members that are available for pylon interfaces. |
タイプ#
名前 | |
---|---|
enum | CxpLinkConfigurationEnums { CxpLinkConfiguration_Auto, CxpLinkConfiguration_CXP10_X1, CxpLinkConfiguration_CXP12_X1, CxpLinkConfiguration_CXP1_X1, CxpLinkConfiguration_CXP2_X1, CxpLinkConfiguration_CXP3_X1, CxpLinkConfiguration_CXP5_X1, CxpLinkConfiguration_CXP6_X1} Valid values for CxpLinkConfiguration. |
enum | CxpPoCxpStatusEnums { CxpPoCxpStatus_Auto, CxpPoCxpStatus_Off, CxpPoCxpStatus_Tripped} Valid values for CxpPoCxpStatus. |
enum | CxpPort0PowerStateEnums { CxpPort0PowerState_AdcFault, CxpPort0PowerState_Disabled, CxpPort0PowerState_HighCurrent, CxpPort0PowerState_HighVoltage, CxpPort0PowerState_Initializing, CxpPort0PowerState_InvalidValue, CxpPort0PowerState_LowVoltage, CxpPort0PowerState_On} Valid values for CxpPort0PowerState. |
enum | CxpPort1PowerStateEnums { CxpPort1PowerState_AdcFault, CxpPort1PowerState_Disabled, CxpPort1PowerState_HighCurrent, CxpPort1PowerState_HighVoltage, CxpPort1PowerState_Initializing, CxpPort1PowerState_InvalidValue, CxpPort1PowerState_LowVoltage, CxpPort1PowerState_On} Valid values for CxpPort1PowerState. |
enum | CxpPort2PowerStateEnums { CxpPort2PowerState_AdcFault, CxpPort2PowerState_Disabled, CxpPort2PowerState_HighCurrent, CxpPort2PowerState_HighVoltage, CxpPort2PowerState_Initializing, CxpPort2PowerState_InvalidValue, CxpPort2PowerState_LowVoltage, CxpPort2PowerState_On} Valid values for CxpPort2PowerState. |
enum | CxpPort3PowerStateEnums { CxpPort3PowerState_AdcFault, CxpPort3PowerState_Disabled, CxpPort3PowerState_HighCurrent, CxpPort3PowerState_HighVoltage, CxpPort3PowerState_Initializing, CxpPort3PowerState_InvalidValue, CxpPort3PowerState_LowVoltage, CxpPort3PowerState_On} Valid values for CxpPort3PowerState. |
enum | DeviceAccessStatusEnums { DeviceAccessStatus_Busy, DeviceAccessStatus_NoAccess, DeviceAccessStatus_OpenReadOnly, DeviceAccessStatus_OpenReadWrite, DeviceAccessStatus_ReadOnly, DeviceAccessStatus_ReadWrite, DeviceAccessStatus_Unknown} Valid values for DeviceAccessStatus. |
enum | DiscoveryMethodEnums { DiscoveryMethod_CameraDiscovery, DiscoveryMethod_EmulationDiscovery, DiscoveryMethod_MixedDiscovery} Valid values for DiscoveryMethod. |
enum | EventNotificationEnums { EventNotification_Off, EventNotification_On, EventNotification_Once} Valid values for EventNotification. |
enum | EventSelectorEnums { EventSelector_DeviceListChanged, EventSelector_InterfaceLost, EventSelector_Line0FallingEdge, EventSelector_Line0RisingEdge, EventSelector_Line1FallingEdge, EventSelector_Line1RisingEdge, EventSelector_Line2FallingEdge, EventSelector_Line2RisingEdge, EventSelector_Line3FallingEdge, EventSelector_Line3RisingEdge, EventSelector_Line4FallingEdge, EventSelector_Line4RisingEdge, EventSelector_Line5FallingEdge, EventSelector_Line5RisingEdge, EventSelector_Line6FallingEdge, EventSelector_Line6RisingEdge, EventSelector_Line7FallingEdge, EventSelector_Line7RisingEdge, EventSelector_LineFront0FallingEdge, EventSelector_LineFront0RisingEdge, EventSelector_LineFront1FallingEdge, EventSelector_LineFront1RisingEdge, EventSelector_LineFront2FallingEdge, EventSelector_LineFront2RisingEdge, EventSelector_LineFront3FallingEdge, EventSelector_LineFront3RisingEdge} Valid values for EventSelector. |
enum | InterfaceAppletEnums { InterfaceApplet_Acq_DualCXP12Area, InterfaceApplet_Acq_DualCXP12Line, InterfaceApplet_Acq_QuadCXP12Area, InterfaceApplet_Acq_QuadCXP12Line, InterfaceApplet_Acq_SingleCXP12Area, InterfaceApplet_Acq_SingleCXP12Line, InterfaceApplet_Acq_SingleCXP12x1Area, InterfaceApplet_Acq_SingleCXP12x1Area_01, InterfaceApplet_Acq_SingleCXP12x1Area_02, InterfaceApplet_Acq_TripleCXP12Area, InterfaceApplet_Acq_TripleCXP12Line, InterfaceApplet_FrameGrabberTest} Valid values for InterfaceApplet. |
enum | InterfaceAppletStatusEnums { InterfaceAppletStatus_Acq_DualCXP12Area, InterfaceAppletStatus_Acq_DualCXP12Line, InterfaceAppletStatus_Acq_QuadCXP12Area, InterfaceAppletStatus_Acq_QuadCXP12Line, InterfaceAppletStatus_Acq_SingleCXP12Area, InterfaceAppletStatus_Acq_SingleCXP12Line, InterfaceAppletStatus_Acq_TripleCXP12Area, InterfaceAppletStatus_Acq_TripleCXP12Line, InterfaceAppletStatus_FrameGrabberTest, InterfaceAppletStatus_Loading, InterfaceAppletStatus_NotLoaded} Valid values for InterfaceAppletStatus. |
enum | InterfaceTypeEnums { InterfaceType_CL, InterfaceType_CLHS, InterfaceType_CXP, InterfaceType_CameraLink, InterfaceType_CameraLinkHS, InterfaceType_CoaXPress, InterfaceType_Custom, InterfaceType_GEV, InterfaceType_GigEVision, InterfaceType_Mixed, InterfaceType_U3V, InterfaceType_USB3Vision} Valid values for InterfaceType. |
Types Documentation#
enum CxpLinkConfigurationEnums#
Enumerator | 値 | 説明 |
---|---|---|
CxpLinkConfiguration_Auto | Link speed is controlled automatically. | |
CxpLinkConfiguration_CXP10_X1 | 1 connection is operating at CXP-10 speed (10 0 Gbps) | |
CxpLinkConfiguration_CXP12_X1 | 1 connection is operating at CXP-12 speed (12 50 Gbps) | |
CxpLinkConfiguration_CXP1_X1 | 1 connection is operating at CXP-1 speed (1 25 Gbps) | |
CxpLinkConfiguration_CXP2_X1 | 1 connection is operating at CXP-2 speed (2 50 Gbps) | |
CxpLinkConfiguration_CXP3_X1 | 1 connection is operating at CXP-3 speed (3 125 Gbps) | |
CxpLinkConfiguration_CXP5_X1 | 1 connection is operating at CXP-5 speed (5 00 Gbps) | |
CxpLinkConfiguration_CXP6_X1 | 1 connection is operating at CXP-6 speed (6 25 Gbps) |
enum CxpPoCxpStatusEnums#
Enumerator | 値 | 説明 |
---|---|---|
CxpPoCxpStatus_Auto | PoCXP operation is set to automatic. | |
CxpPoCxpStatus_Off | PoCXP is forced off. | |
CxpPoCxpStatus_Tripped | The link has shut down because of an over-current trip. |
Valid values for CxpPoCxpStatus.
enum CxpPort0PowerStateEnums#
Enumerator | 値 | 説明 |
---|---|---|
CxpPort0PowerState_AdcFault | The PoCXP state can't be determined because of an A/D converter fault. | |
CxpPort0PowerState_Disabled | PoCXP is disabled. | |
CxpPort0PowerState_HighCurrent | PoCXP is off because of an over current trip. | |
CxpPort0PowerState_HighVoltage | PoCXP is off because the voltage is too high. | |
CxpPort0PowerState_Initializing | The PoCXP state machine is looking for devices. | |
CxpPort0PowerState_InvalidValue | The PoCXP state can't be determined. | |
CxpPort0PowerState_LowVoltage | PoCXP is off because the voltage is too low. | |
CxpPort0PowerState_On | PoCXP is active. |
Valid values for CxpPort0PowerState.
enum CxpPort1PowerStateEnums#
Enumerator | 値 | 説明 |
---|---|---|
CxpPort1PowerState_AdcFault | The PoCXP state can't be determined because of an A/D converter fault. | |
CxpPort1PowerState_Disabled | PoCXP is disabled. | |
CxpPort1PowerState_HighCurrent | PoCXP is off because of an over current trip. | |
CxpPort1PowerState_HighVoltage | PoCXP is off because the voltage is too high. | |
CxpPort1PowerState_Initializing | The PoCXP state machine is looking for devices. | |
CxpPort1PowerState_InvalidValue | The PoCXP state can't be determined. | |
CxpPort1PowerState_LowVoltage | PoCXP is off because the voltage is too low. | |
CxpPort1PowerState_On | PoCXP is active. |
Valid values for CxpPort1PowerState.
enum CxpPort2PowerStateEnums#
Enumerator | 値 | 説明 |
---|---|---|
CxpPort2PowerState_AdcFault | The PoCXP state can't be determined because of an A/D converter fault. | |
CxpPort2PowerState_Disabled | PoCXP is disabled. | |
CxpPort2PowerState_HighCurrent | PoCXP is off because of an over current trip. | |
CxpPort2PowerState_HighVoltage | PoCXP is off because the voltage is too high. | |
CxpPort2PowerState_Initializing | The PoCXP state machine is looking for devices. | |
CxpPort2PowerState_InvalidValue | The PoCXP state can't be determined. | |
CxpPort2PowerState_LowVoltage | PoCXP is off because the voltage is too low. | |
CxpPort2PowerState_On | PoCXP is active. |
Valid values for CxpPort2PowerState.
enum CxpPort3PowerStateEnums#
Enumerator | 値 | 説明 |
---|---|---|
CxpPort3PowerState_AdcFault | The PoCXP state can't be determined because of an A/D converter fault. | |
CxpPort3PowerState_Disabled | PoCXP is disabled. | |
CxpPort3PowerState_HighCurrent | PoCXP is off because of an over current trip. | |
CxpPort3PowerState_HighVoltage | PoCXP is off because the voltage is too high. | |
CxpPort3PowerState_Initializing | The PoCXP state machine is looking for devices. | |
CxpPort3PowerState_InvalidValue | The PoCXP state can't be determined. | |
CxpPort3PowerState_LowVoltage | PoCXP is off because the voltage is too low. | |
CxpPort3PowerState_On | PoCXP is active. |
Valid values for CxpPort3PowerState.
enum DeviceAccessStatusEnums#
Enumerator | 値 | 説明 |
---|---|---|
DeviceAccessStatus_Busy | The device is already opened by another entity. | |
DeviceAccessStatus_NoAccess | You can't connect to the device. | |
DeviceAccessStatus_OpenReadOnly | The device is opened in Read-only mode by this GenTL host. | |
DeviceAccessStatus_OpenReadWrite | The device is opened in Read/Write mode by this GenTL host. | |
DeviceAccessStatus_ReadOnly | The device offers read-only access. | |
DeviceAccessStatus_ReadWrite | The device offers read/write access. | |
DeviceAccessStatus_Unknown | The status is unknown. |
Valid values for DeviceAccessStatus.
enum DiscoveryMethodEnums#
Enumerator | 値 | 説明 |
---|---|---|
DiscoveryMethod_CameraDiscovery | Discover only real cameras as remote devices. | |
DiscoveryMethod_EmulationDiscovery | Discover only emulated cameras as remote devices. | |
DiscoveryMethod_MixedDiscovery | Discover real cameras and remote devices when no real cameras are present. |
Valid values for DiscoveryMethod.
enum EventNotificationEnums#
Enumerator | 値 | 説明 |
---|---|---|
EventNotification_Off | The selected event notification is disabled. | |
EventNotification_On | The selected event notification is enabled. | |
EventNotification_Once | The selected event notification is enabled for one event and then returned to Off state. |
Valid values for EventNotification.
enum EventSelectorEnums#
Enumerator | 値 | 説明 |
---|---|---|
EventSelector_DeviceListChanged | The DeviceListChanged event is selected. | |
EventSelector_InterfaceLost | The Interface Lost event is selected. | |
EventSelector_Line0FallingEdge | Entry for the event Line0FallingEdge. | |
EventSelector_Line0RisingEdge | Entry for the event Line0RisingEdge. | |
EventSelector_Line1FallingEdge | Entry for the event Line1FallingEdge. | |
EventSelector_Line1RisingEdge | Entry for the event Line1RisingEdge. | |
EventSelector_Line2FallingEdge | Entry for the event Line2FallingEdge. | |
EventSelector_Line2RisingEdge | Entry for the event Line2RisingEdge. | |
EventSelector_Line3FallingEdge | Entry for the event Line3FallingEdge. | |
EventSelector_Line3RisingEdge | Entry for the event Line3RisingEdge. | |
EventSelector_Line4FallingEdge | Entry for the event Line4FallingEdge. | |
EventSelector_Line4RisingEdge | Entry for the event Line4RisingEdge. | |
EventSelector_Line5FallingEdge | Entry for the event Line5FallingEdge. | |
EventSelector_Line5RisingEdge | Entry for the event Line5RisingEdge. | |
EventSelector_Line6FallingEdge | Entry for the event Line6FallingEdge. | |
EventSelector_Line6RisingEdge | Entry for the event Line6RisingEdge. | |
EventSelector_Line7FallingEdge | Entry for the event Line7FallingEdge. | |
EventSelector_Line7RisingEdge | Entry for the event Line7RisingEdge. | |
EventSelector_LineFront0FallingEdge | Entry for the event LineFront0FallingEdge. | |
EventSelector_LineFront0RisingEdge | Entry for the event LineFront0RisingEdge. | |
EventSelector_LineFront1FallingEdge | Entry for the event LineFront1FallingEdge. | |
EventSelector_LineFront1RisingEdge | Entry for the event LineFront1RisingEdge. | |
EventSelector_LineFront2FallingEdge | Entry for the event LineFront2FallingEdge. | |
EventSelector_LineFront2RisingEdge | Entry for the event LineFront2RisingEdge. | |
EventSelector_LineFront3FallingEdge | Entry for the event LineFront3FallingEdge. | |
EventSelector_LineFront3RisingEdge | Entry for the event LineFront3RisingEdge. |
Valid values for EventSelector.
enum InterfaceAppletEnums#
Enumerator | 値 | 説明 |
---|---|---|
InterfaceApplet_Acq_DualCXP12Area | The Acq_DualCXP12Area applet is used to initialize the interface. | |
InterfaceApplet_Acq_DualCXP12Line | ||
InterfaceApplet_Acq_QuadCXP12Area | The Acq_QuadCXP12Area applet is used to initialize the interface. | |
InterfaceApplet_Acq_QuadCXP12Line | ||
InterfaceApplet_Acq_SingleCXP12Area | The Acq_SingleCXP12Area applet is used to initialize the interface. | |
InterfaceApplet_Acq_SingleCXP12Line | ||
InterfaceApplet_Acq_SingleCXP12x1Area | The Acq_SingleCXP12x1Area applet is used to initialize the interface. | |
InterfaceApplet_Acq_SingleCXP12x1Area_01 | The Acq_SingleCXP12x1Area_01 applet is used to initialize the interface. | |
InterfaceApplet_Acq_SingleCXP12x1Area_02 | The Acq_SingleCXP12x1Area_02 applet is used to initialize the interface. | |
InterfaceApplet_Acq_TripleCXP12Area | The Acq_TripleCXP12Area applet is used to initialize the interface. | |
InterfaceApplet_Acq_TripleCXP12Line | ||
InterfaceApplet_FrameGrabberTest |
Valid values for InterfaceApplet.
enum InterfaceAppletStatusEnums#
Enumerator | 値 | 説明 |
---|---|---|
InterfaceAppletStatus_Acq_DualCXP12Area | The status of the Acq_DualCXP12Area applet is returned. | |
InterfaceAppletStatus_Acq_DualCXP12Line | ||
InterfaceAppletStatus_Acq_QuadCXP12Area | The status of the Acq_QuadCXP12Area applet is returned. | |
InterfaceAppletStatus_Acq_QuadCXP12Line | ||
InterfaceAppletStatus_Acq_SingleCXP12Area | The status of the Acq_SingleCXP12Area applet is returned. | |
InterfaceAppletStatus_Acq_SingleCXP12Line | ||
InterfaceAppletStatus_Acq_TripleCXP12Area | The status of the Acq_TripleCXP12Area applet is returned. | |
InterfaceAppletStatus_Acq_TripleCXP12Line | ||
InterfaceAppletStatus_FrameGrabberTest | ||
InterfaceAppletStatus_Loading | The status of the applet is Loading. | |
InterfaceAppletStatus_NotLoaded | The status of the applet is NotLoaded. |
Valid values for InterfaceAppletStatus.
enum InterfaceTypeEnums#
Enumerator | 値 | 説明 |
---|---|---|
InterfaceType_CL | The interface uses the Camera Link transport layer. | |
InterfaceType_CLHS | The interface uses the Camera Link HS transport layer. | |
InterfaceType_CXP | The interface uses the CoaXPress transport layer. | |
InterfaceType_CameraLink | Camera Link. | |
InterfaceType_CameraLinkHS | Camera Link High Speed. | |
InterfaceType_CoaXPress | CoaXPress. | |
InterfaceType_Custom | The interface uses a custom transport layer. | |
InterfaceType_GEV | The interface uses the GigE Vision transport layer. | |
InterfaceType_GigEVision | GigE Vision. | |
InterfaceType_Mixed | Different interface modules of the GenTL Producer are of different types. | |
InterfaceType_U3V | The interface uses the USB3 Vision transport layer. | |
InterfaceType_USB3Vision | USB3 Vision. |
Valid values for InterfaceType.