PLCamera.BLCSerialTransmitQueueStatusEnum Class#
Applies to: GigE and ace USB
Visibility: Guru
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BLCSerialTransmitQueueStatusEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BLCSerialTransmitQueueStatusEnum | Initializes a new instance of the PLCamera.BLCSerialTransmitQueueStatusEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Empty | The transmit queue is empty. Applies to: GigE and ace USB | |
Filled | The transmit queue contains at least one value. Applies to: GigE and ace USB | |
Full | The transmit queue is full. Applies to: GigE and ace USB | |
名前 | The full name of BLCSerialTransmitQueueStatus (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BLCSerialTransmitQueueStatus (Overrides Object.ToString()()()().) |
PLCamera.BLCSerialTransmitQueueStatusEnum.ToString Method#
The full name of BLCSerialTransmitQueueStatus
Return Value#
Type: String
Returns the full name of BLCSerialTransmitQueueStatus
PLCamera.BLCSerialTransmitQueueStatusEnum Constructor#
Initializes a new instance of the PLCamera.BLCSerialTransmitQueueStatusEnum class
PLCamera.BLCSerialTransmitQueueStatusEnum.Empty Property#
The transmit queue is empty.
Applies to: GigE and ace USB
PLCamera.BLCSerialTransmitQueueStatusEnum.Filled Property#
The transmit queue contains at least one value.
Applies to: GigE and ace USB
PLCamera.BLCSerialTransmitQueueStatusEnum.Full Property#
The transmit queue is full.
Applies to: GigE and ace USB
PLCamera.BLCSerialTransmitQueueStatusEnum.Name Property#
The full name of BLCSerialTransmitQueueStatus