PLTransportLayer.TriggerInStatisticsPolarityEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerInStatisticsPolarityEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.TriggerInStatisticsPolarityEnum | Initializes a new instance of the PLTransportLayer.TriggerInStatisticsPolarityEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
HighActive | The trigger polarity of the input specified by the Statistics Source parameter is set to High Active. Applies to: CoaXPress | |
LowActive | The trigger polarity of the input specified by the Statistics Source parameter is set to Low Active. Applies to: CoaXPress | |
名前 | The full name of TriggerInStatisticsPolarity (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerInStatisticsPolarity (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerInStatisticsPolarityEnum.ToString Method#
The full name of TriggerInStatisticsPolarity
Return Value#
Type: String
Returns the full name of TriggerInStatisticsPolarity
PLTransportLayer.TriggerInStatisticsPolarityEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerInStatisticsPolarityEnum class
PLTransportLayer.TriggerInStatisticsPolarityEnum.HighActive Property#
The trigger polarity of the input specified by the Statistics Source parameter is set to High Active.
Applies to: CoaXPress
PLTransportLayer.TriggerInStatisticsPolarityEnum.LowActive Property#
The trigger polarity of the input specified by the Statistics Source parameter is set to Low Active.
Applies to: CoaXPress
PLTransportLayer.TriggerInStatisticsPolarityEnum.Name Property#
The full name of TriggerInStatisticsPolarity